Part Number: AM4378
HI,
In my project I need to write video file on eMMC in real time.
To do this I need 30 MB/s of sequential write data rate then normal 4GB eMMC aren't usable.
I found the Sandisk iNAND 7250 , 8GB, 40MB/s that it seems to be compatible with Sitara:
3,3V , HS200 interface ...
The eMMC must also do Linux boot.
Someone can confirm to me that iNAND is compatible with requested performances ?
Thks