This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: USB intermittent failures

Part Number: PROCESSOR-SDK-AM335X

Tool/software: Linux

Hi

hello guys i am using custom beagle bone black with TI SDK

  1. now sometimes the usb drivers fail to boot up
  2. out of 10 times 7 times USB drivers boot sucessfully 3 times usb drivers fails to boot

i am attaching the dmesg of both fails boot up and successfull boot up can you please let me know the  permanent solution for this

it shows some strange error in the fail attempt : [   12.906464] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517

2061.config.txt

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Initializing cgroup subsys cpu
[    0.000000] Initializing cgroup subsys cpuacct
[    0.000000] Linux version 4.4.41+ (gitlab-runner@nick-NUC7i7BNHXG) (gcc version 6.2.1 20161016 (Linaro GCC 6.2-2016.11) ) #12 PREEMPT Tue May 1 17:35:09 BST 2018
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine model: TI AM335x BeagleBone Black
[    0.000000] cma: Reserved 48 MiB at 0x9d000000
[    0.000000] Memory policy: Data cache writeback
[    0.000000] On node 0 totalpages: 131072
[    0.000000] free_area_init_node: node 0, pgdat c092a90c, node_mem_map dcb61000
[    0.000000]   Normal zone: 1152 pages used for memmap
[    0.000000]   Normal zone: 0 pages reserved
[    0.000000]   Normal zone: 131072 pages, LIFO batch:31
[    0.000000] CPU: All CPU(s) started in SVC mode.
[    0.000000] AM335X ES2.1 (sgx neon )
[    0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[    0.000000] pcpu-alloc: [0] 0
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 129920
[    0.000000] Kernel command line: console=/dev/null root=PARTUUID=bf388b61-02 rw rootfstype=ext4 rootwait
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Memory: 460164K/524288K available (6603K kernel code, 266K rwdata, 2228K rodata, 260K init, 265K bss, 14972K reserved, 49152K cma-reserved, 0K highmem)
[    0.000000] Virtual kernel memory layout:
                   vector  : 0xffff0000 - 0xffff1000   (   4 kB)
                   fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
                   vmalloc : 0xe0800000 - 0xff800000   ( 496 MB)
                   lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
                   pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
                   modules : 0xbf000000 - 0xbfe00000   (  14 MB)
                     .text : 0xc0008000 - 0xc08a800c   (8833 kB)
                     .init : 0xc08a9000 - 0xc08ea000   ( 260 kB)
                     .data : 0xc08ea000 - 0xc092cad8   ( 267 kB)
                      .bss : 0xc092cad8 - 0xc096f25c   ( 266 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000] 	Build-time adjustment of leaf fanout to 32.
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[    0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[    0.000013] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[    0.000032] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[    0.000041] OMAP clocksource: timer1 at 24000000 Hz
[    0.000182] clocksource_probe: no matching clocksources found
[    0.000338] Console: colour dummy device 80x30
[    0.000374] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[    0.089272] pid_max: default: 32768 minimum: 301
[    0.089369] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.089379] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.089965] Initializing cgroup subsys io
[    0.089992] Initializing cgroup subsys memory
[    0.090024] Initializing cgroup subsys devices
[    0.090038] Initializing cgroup subsys freezer
[    0.090050] Initializing cgroup subsys perf_event
[    0.090060] Initializing cgroup subsys pids
[    0.090083] CPU: Testing write buffer coherency: ok
[    0.090443] Setting up static identity map for 0x80008200 - 0x80008260
[    0.092257] devtmpfs: initialized
[    0.102313] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[    0.115215] omap_hwmod: debugss: _wait_target_disable failed
[    0.169933] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.173382] pinctrl core: initialized pinctrl subsystem
[    0.174569] NET: Registered protocol family 16
[    0.176422] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.199263] cpuidle: using governor ladder
[    0.229253] cpuidle: using governor menu
[    0.232744] gpiochip_add: registered GPIOs 0 to 31 on device: gpio
[    0.233015] OMAP GPIO hardware version 0.1
[    0.233673] gpiochip_add: registered GPIOs 32 to 63 on device: gpio
[    0.234330] gpiochip_add: registered GPIOs 64 to 95 on device: gpio
[    0.234971] gpiochip_add: registered GPIOs 96 to 127 on device: gpio
[    0.242356] hw-breakpoint: debug architecture 0x4 unsupported.
[    0.276260] edma 49000000.edma: TI EDMA DMA engine driver
[    0.276600] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator@0[0]'
[    0.279070] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[    0.279125] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/i2c1_pins, deferring probe
[    0.279379] media: Linux media interface: v0.10
[    0.279442] Linux video capture interface: v2.00
[    0.279494] pps_core: LinuxPPS API ver. 1 registered
[    0.279501] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.279525] PTP clock support registered
[    0.279577] EDAC MC: Ver: 3.0.0
[    0.280582] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[    0.280929] Advanced Linux Sound Architecture Driver Initialized.
[    0.281928] clocksource: Switched to clocksource timer1
[    0.290974] NET: Registered protocol family 2
[    0.291659] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[    0.291703] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[    0.291741] TCP: Hash tables configured (established 4096 bind 4096)
[    0.291807] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.291823] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.292009] NET: Registered protocol family 1
[    0.292379] RPC: Registered named UNIX socket transport module.
[    0.292391] RPC: Registered udp transport module.
[    0.292395] RPC: Registered tcp transport module.
[    0.292401] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.292429] PCI: CLS 0 bytes, default 64
[    0.293248] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[    0.294924] futex hash table entries: 256 (order: -1, 3072 bytes)
[    0.301358] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.302161] NFS: Registering the id_resolver key type
[    0.302223] Key type id_resolver registered
[    0.302230] Key type id_legacy registered
[    0.302291] ntfs: driver 2.1.32 [Flags: R/O].
[    0.303945] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[    0.303968] io scheduler noop registered
[    0.303979] io scheduler deadline registered
[    0.304009] io scheduler cfq registered (default)
[    0.305231] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[    0.307920] pwm-backlight backlight: GPIO lookup for consumer enable
[    0.307941] pwm-backlight backlight: using device tree for GPIO lookup
[    0.307954] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/backlight[0]'
[    0.307963] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/backlight[0]'
[    0.307971] pwm-backlight backlight: using lookup tables for GPIO lookup
[    0.307980] pwm-backlight backlight: lookup for GPIO enable failed
[    0.308000] backlight supply power not found, using dummy regulator
[    0.358732] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[    0.362405] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[    0.363466] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 159, base_baud = 3000000) is a 8250
[    0.364425] 48024000.serial: ttyS2 at MMIO 0x48024000 (irq = 160, base_baud = 3000000) is a 8250
[    0.365330] 481a8000.serial: ttyS4 at MMIO 0x481a8000 (irq = 161, base_baud = 3000000) is a 8250
[    0.366981] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[    0.367111] [drm] Initialized drm 1.1.0 20060810
[    0.378077] brd: module loaded
[    0.383549] loop: module loaded
[    0.387046] libphy: Fixed MDIO Bus: probed
[    0.452001] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[    0.452021] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[    0.452873] libphy: 4a101000.mdio: probed
[    0.452898] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720
[    0.453497] cpsw 4a100000.ethernet: Detected MACID = 2c:6b:7d:5a:3f:86
[    0.453616] cpsw 4a100000.ethernet: cpts: overflow check period 850
[    0.454876] mousedev: PS/2 mouse device common for all mice
[    0.455370] i2c /dev entries driver
[    0.456423] cpuidle: enable-method property 'ti,am3352' found operations
[    0.457023] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[    0.457038] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[    0.457064] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp/mmc@48060000[0]' - status (0)
[    0.457135] omap_hsmmc 48060000.mmc: Got CD GPIO
[    0.457149] omap_hsmmc 48060000.mmc: GPIO lookup for consumer wp
[    0.457156] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[    0.457165] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@48060000[0]'
[    0.457174] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@48060000[0]'
[    0.457182] omap_hsmmc 48060000.mmc: using lookup tables for GPIO lookup
[    0.457190] omap_hsmmc 48060000.mmc: lookup for GPIO wp failed
[    0.492459] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer cd
[    0.492477] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
[    0.492490] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp/mmc@481d8000[0]'
[    0.492498] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp/mmc@481d8000[0]'
[    0.492587] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
[    0.492599] omap_hsmmc 481d8000.mmc: lookup for GPIO cd failed
[    0.492610] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer wp
[    0.492617] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
[    0.492625] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@481d8000[0]'
[    0.492633] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@481d8000[0]'
[    0.492641] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
[    0.492648] omap_hsmmc 481d8000.mmc: lookup for GPIO wp failed
[    0.532516] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@2[0]' - status (0)
[    0.532746] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@3[0]' - status (0)
[    0.532867] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@4[0]' - status (0)
[    0.532969] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@5[0]' - status (0)
[    0.533399] ledtrig-cpu: registered to indicate activity on CPUs
[    0.537182] NET: Registered protocol family 10
[    0.540423] sit: IPv6 over IPv4 tunneling driver
[    0.541122] NET: Registered protocol family 17
[    0.541410] Key type dns_resolver registered
[    0.541630] omap_voltage_late_init: Voltage driver support not added
[    0.568970] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[    0.569222] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[    0.569263] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[    0.570225] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 100 kHz
[    0.572332] of_get_named_gpiod_flags: parsed 'gpios' property of node '/wakeup_keys@0/test@0[0]' - status (0)
[    0.572368] of_get_named_gpiod_flags: parsed 'gpios' property of node '/wakeup_keys@0/test@1[0]' - status (0)
[    0.572821] input: wakeup_keys@0 as /devices/platform/wakeup_keys@0/input/input0
[    0.573269] hctosys: unable to open rtc device (rtc0)
[    0.576169] mmc1: MAN_BKOPS_EN bit is not set
[    0.576733] ALSA device list:
[    0.576747]   No soundcards found.
[    0.576873] Warning: unable to open an initial console.
[    0.577075] Waiting for root device PARTUUID=bf388b61-02...
[    0.579973] mmc1: new high speed MMC card at address 0001
[    0.580660] mmcblk0: mmc1:0001 MMC04G 3.52 GiB
[    0.580879] mmcblk0boot0: mmc1:0001 MMC04G partition 1 16.0 MiB
[    0.581104] mmcblk0boot1: mmc1:0001 MMC04G partition 2 16.0 MiB
[    0.583221]  mmcblk0: p1 p2
[    0.707514] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    0.707591] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    0.715768] devtmpfs: mounted
[    0.716063] Freeing unused kernel memory: 260K (c08a9000 - c08ea000)
[    0.716070] This architecture does not have kernel memory protection.
[    1.050677] systemd[1]: System time before build time, advancing clock.
[    1.125165] random: systemd: uninitialized urandom read (16 bytes read, 15 bits of entropy available)
[    1.133442] random: systemd: uninitialized urandom read (16 bytes read, 15 bits of entropy available)
[    1.160450] systemd[1]: systemd 230 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[    1.161766] systemd[1]: Detected architecture arm.
[    1.183809] systemd[1]: Set hostname to <scada>.
[    1.268498] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 18 bits of entropy available)
[    1.268975] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 18 bits of entropy available)
[    1.298355] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 18 bits of entropy available)
[    1.310534] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 19 bits of entropy available)
[    1.319471] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
[    1.411283] random: systemd: uninitialized urandom read (16 bytes read, 23 bits of entropy available)
[    1.411691] random: systemd: uninitialized urandom read (16 bytes read, 23 bits of entropy available)
[    1.413958] random: systemd: uninitialized urandom read (16 bytes read, 23 bits of entropy available)
[    1.475660] systemd[1]: [/lib/systemd/system/gadget-init.service:15] Unknown lvalue 'ExecStopPre' in section 'Service'
[    1.737885] systemd[1]: sysinit.target: Found ordering cycle on sysinit.target/start
[    1.737938] systemd[1]: sysinit.target: Found dependency on alignment.service/start
[    1.737966] systemd[1]: sysinit.target: Found dependency on basic.target/start
[    1.737987] systemd[1]: sysinit.target: Found dependency on sysinit.target/start
[    1.738009] systemd[1]: sysinit.target: Breaking ordering cycle by deleting job alignment.service/start
[    1.738033] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with sysinit.target/start
[    1.744726] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[    1.745214] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[    1.745665] systemd[1]: Listening on udev Control Socket.
[    1.747824] systemd[1]: Created slice System Slice.
[    1.749149] systemd[1]: Created slice system-serial\x2dgetty.slice.
[    1.749572] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[    1.749745] systemd[1]: Reached target Paths.
[    1.750045] systemd[1]: Listening on udev Kernel Socket.
[    1.750402] systemd[1]: Listening on Syslog Socket.
[    1.750567] systemd[1]: Reached target Remote File Systems.
[    1.750827] systemd[1]: Listening on Journal Socket (/dev/log).
[    1.752185] systemd[1]: Created slice User and Session Slice.
[    1.752407] systemd[1]: Reached target Slices.
[    1.753024] systemd[1]: Listening on Network Service Netlink Socket.
[    1.754334] systemd[1]: Created slice system-getty.slice.
[    1.754523] systemd[1]: Reached target Swap.
[    1.779621] systemd[1]: Listening on Journal Socket.
[    1.795549] systemd[1]: Starting Load Kernel Modules...
[    1.800278] systemd[1]: Starting Setup Virtual Console...
[    1.824813] systemd[1]: Mounting Debug File System...
[    1.861592] systemd[1]: Mounting Temporary Directory...
[    1.916482] systemd[1]: Starting Journal Service...
[    1.960544] systemd[1]: Starting Create Static Device Nodes in /dev...
[    1.971817] systemd[1]: Mounting POSIX Message Queue File System...
[    2.059694] systemd[1]: Starting Remount Root and Kernel File Systems...
[    2.130064] systemd[1]: Mounted Debug File System.
[    2.130399] systemd[1]: Mounted POSIX Message Queue File System.
[    2.130589] systemd[1]: Mounted Temporary Directory.
[    2.141059] usbcore: registered new interface driver usbfs
[    2.141153] usbcore: registered new interface driver hub
[    2.156042] usbcore: registered new device driver usb
[    2.170815] systemd[1]: Started Setup Virtual Console.
[    2.215891] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[    2.250776] systemd[1]: Started Create Static Device Nodes in /dev.
[    2.253489] systemd[1]: Started Remount Root and Kernel File Systems.
[    2.265848] usbcore: registered new interface driver ath9k_htc
[    2.286230] systemd[1]: Starting udev Coldplug all Devices...
[    2.290670] systemd[1]: Starting udev Kernel Device Manager...
[    2.290888] systemd[1]: Reached target Local File Systems (Pre).
[    2.306242] ip_tables: (C) 2000-2006 Netfilter Core Team
[    2.337036] systemd[1]: Mounting /media/ram...
[    2.340901] systemd[1]: Mounting /var/volatile...
[    2.357470] nf_conntrack version 0.5.0 (7962 buckets, 31848 max)
[    2.471505] systemd[1]: Mounted /var/volatile.
[    2.471871] systemd[1]: Mounted /media/ram.
[    2.483106] systemd[1]: Started Journal Service.
[    2.744152] systemd-journald[98]: Received request to flush runtime journal from PID 1
[    3.224491] cfg80211: World regulatory domain updated:
[    3.224527] cfg80211:  DFS Master region: unset
[    3.224537] cfg80211:   (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)
[    3.224550] cfg80211:   (2402000 KHz - 2472000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)
[    3.224561] cfg80211:   (2457000 KHz - 2482000 KHz @ 20000 KHz, 92000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[    3.224569] cfg80211:   (2474000 KHz - 2494000 KHz @ 20000 KHz), (N/A, 2000 mBm), (N/A)
[    3.224578] cfg80211:   (5170000 KHz - 5250000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[    3.224587] cfg80211:   (5250000 KHz - 5330000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (0 s)
[    3.224595] cfg80211:   (5490000 KHz - 5730000 KHz @ 160000 KHz), (N/A, 2000 mBm), (0 s)
[    3.224603] cfg80211:   (5735000 KHz - 5835000 KHz @ 80000 KHz), (N/A, 2000 mBm), (N/A)
[    3.224610] cfg80211:   (57240000 KHz - 63720000 KHz @ 2160000 KHz), (N/A, 0 mBm), (N/A)
[    4.438443] omap_rtc 44e3e000.rtc: already running
[    4.447807] TI-am335x-tsc TI-am335x-tsc: ti,charge-delay not specified
[    4.448138] input: ti-tsc as /devices/platform/ocp/44e0d000.tscadc/TI-am335x-tsc/input/input1
[    4.448793] rtc rtc0: 44e3e000.rtc: dev (254:0)
[    4.448826] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[    4.556308] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    4.945141] CAN device driver interface
[    5.029506] c_can_platform 481cc000.can: c_can_platform device registered (regs=fa1cc000, irq=167)
[    5.331521] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[    5.411030] ti-pruss 4a300000.pruss: creating PRU cores and other child platform devices
[    5.412681] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[    5.413243] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[    5.413769] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[    5.489777]  remoteproc0: 4a334000.pru0 is available
[    5.489805]  remoteproc0: Note: remoteproc is still under development and considered experimental.
[    5.489813]  remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[    5.499316]  remoteproc0: registered virtio0 (type 7)
[    5.513292]  remoteproc1: wkup_m3 is available
[    5.513319]  remoteproc1: Note: remoteproc is still under development and considered experimental.
[    5.513326]  remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[    5.521542] pru-rproc 4a334000.pru0: PRU rproc node /ocp/pruss@4a300000/pru0@4a334000 probed successfully
[    5.531102]  remoteproc2: 4a338000.pru1 is available
[    5.531133]  remoteproc2: Note: remoteproc is still under development and considered experimental.
[    5.531140]  remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[    5.537975]  remoteproc2: registered virtio1 (type 7)
[    5.538071] pru-rproc 4a338000.pru1: PRU rproc node /ocp/pruss@4a300000/pru1@4a338000 probed successfully
[    5.738382]  remoteproc1: powering up wkup_m3
[    5.739408]  remoteproc1: Booting fw image am335x-pm-firmware.elf, size 224344
[    5.739679]  remoteproc1: remote processor wkup_m3 is now up
[    5.739714] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[    5.799744] PM: bootloader does not support rtc-only!
[    6.680012] net eth0: initializing cpsw version 1.12 (0)
[    6.680065] net eth0: initialized cpsw ale version 1.4
[    6.680075] net eth0: ALE Table size 1024
[    6.715766] net eth0: phy found : id is : 0x7c0f1
[    6.715880] libphy: PHY 4a101000.mdio:01 not found
[    6.715893] net eth0: phy "4a101000.mdio:01" not found on slave 1, err -19
[    6.790866] Bluetooth: Core ver 2.21
[    6.790969] NET: Registered protocol family 31
[    6.790978] Bluetooth: HCI device and connection manager initialized
[    6.791002] Bluetooth: HCI socket layer initialized
[    6.791016] Bluetooth: L2CAP socket layer initialized
[    6.791061] Bluetooth: SCO socket layer initialized
[    6.838497] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[    9.589517] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[    9.634804] NET: Registered protocol family 15
[   10.560555] Initializing XFRM netlink socket
[   10.752862] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[   10.753009] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[   11.062468] random: nonblocking pool is initialized
[   13.399112] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer reset
[   13.399142] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lookup
[   13.399158] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[   13.399168] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[   13.399176] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO lookup
[   13.399185] am335x-phy-driver 47401300.usb-phy: lookup for GPIO reset failed
[   13.399195] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer vbus-detect
[   13.399203] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lookup
[   13.399212] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[   13.399221] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[   13.399229] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO lookup
[   13.399237] am335x-phy-driver 47401300.usb-phy: lookup for GPIO vbus-detect failed
[   13.399301] 47401300.usb-phy supply vcc not found, using dummy regulator
[   13.482865] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer reset
[   13.482896] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lookup
[   13.482913] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[   13.482922] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[   13.482931] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO lookup
[   13.482940] am335x-phy-driver 47401b00.usb-phy: lookup for GPIO reset failed
[   13.482951] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer vbus-detect
[   13.482958] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lookup
[   13.482967] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[   13.482976] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[   13.482984] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO lookup
[   13.482992] am335x-phy-driver 47401b00.usb-phy: lookup for GPIO vbus-detect failed
[   13.483056] 47401b00.usb-phy supply vcc not found, using dummy regulator
[   13.519707] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[   13.519735] musb-hdrc: MHDRC RTL version 2.0
[   13.519742] musb-hdrc: setup fifo_mode 4
[   13.519761] musb-hdrc: 28/31 max ep, 16384/16384 memory
[   13.621900] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[   13.632434] musb-hdrc: MHDRC RTL version 2.0
[   13.632457] musb-hdrc: setup fifo_mode 4
[   13.632477] musb-hdrc: 28/31 max ep, 16384/16384 memory
[   13.632617] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[   13.632650] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 1
[   13.633645] hub 1-0:1.0: USB hub found
[   13.635357] hub 1-0:1.0: 1 port detected
[   13.698156] musb-hdrc musb-hdrc.1.auto: VBUS_ERROR in a_wait_vrise (89, <AValid), retry #1, port1 00000100
[   14.102097] usb 1-1: new high-speed USB device number 2 using musb-hdrc
[   14.245098] hub 1-1:1.0: USB hub found
[   14.245468] hub 1-1:1.0: 4 ports detected
[   14.370470]  remoteproc0: powering up 4a334000.pru0
[   14.370965]  remoteproc0: Booting fw image am335x-pru0-fw, size 75688
[   14.371153] ti-pruss 4a300000.pruss: configured system_events = 0x0000000000030000 intr_channels = 0x00000005 host_intr = 0x00000005
[   14.384845]  remoteproc0: remote processor 4a334000.pru0 is now up
[   14.385191] virtio_rpmsg_bus virtio0: creating channel rpmsg-pru addr 0x1e
[   14.385427] virtio_rpmsg_bus virtio0: rpmsg host is online
[   14.385614]  remoteproc2: powering up 4a338000.pru1
[   14.386110]  remoteproc2: Booting fw image am335x-pru1-fw, size 75688
[   14.386293] ti-pruss 4a300000.pruss: configured system_events = 0x00000000000c0000 intr_channels = 0x0000000a host_intr = 0x0000000a
[   14.398846]  remoteproc2: remote processor 4a338000.pru1 is now up
[   14.399172] virtio_rpmsg_bus virtio1: creating channel rpmsg-pru addr 0x1f
[   14.399420] virtio_rpmsg_bus virtio1: rpmsg host is online
[   14.523595] usb 1-1.3: new high-speed USB device number 3 using musb-hdrc
[   14.643666] usb 1-1.3: ath9k_htc: Firmware ath9k_htc/htc_9271-1.4.0.fw requested
[   14.683782] rpmsg_pru rpmsg0: new rpmsg_pru device: /dev/rpmsg_pru30
[   14.709196] rpmsg_pru rpmsg1: new rpmsg_pru device: /dev/rpmsg_pru31
[   14.929639] usb 1-1.3: ath9k_htc: Transferred FW: ath9k_htc/htc_9271-1.4.0.fw, size: 51008
[   15.180213] ath9k_htc 1-1.3:1.0: ath9k_htc: HTC initialized with 33 credits
[   15.412500] ath9k_htc 1-1.3:1.0: ath9k_htc: FW Version: 1.4
[   15.412529] ath9k_htc 1-1.3:1.0: FW RMW support: On
[   15.412539] ath: EEPROM regdomain: 0x60
[   15.412545] ath: EEPROM indicates we should expect a direct regpair map
[   15.412561] ath: Country alpha2 being used: 00
[   15.412565] ath: Regpair used: 0x60
[   15.427065] ieee80211 phy0: Atheros AR9271 Rev:1
[   19.005286] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[   21.640966] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[   21.981136] cfg80211: Regulatory domain changed to country: US
[   21.981172] cfg80211:  DFS Master region: FCC
[   21.981182] cfg80211:   (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)
[   21.981195] cfg80211:   (2402000 KHz - 2472000 KHz @ 40000 KHz), (N/A, 3000 mBm), (N/A)
[   21.981206] cfg80211:   (5170000 KHz - 5250000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2300 mBm), (N/A)
[   21.981215] cfg80211:   (5250000 KHz - 5330000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2300 mBm), (0 s)
[   21.981223] cfg80211:   (5490000 KHz - 5730000 KHz @ 160000 KHz), (N/A, 2300 mBm), (0 s)
[   21.981231] cfg80211:   (5735000 KHz - 5835000 KHz @ 80000 KHz), (N/A, 3000 mBm), (N/A)
[   21.981239] cfg80211:   (57240000 KHz - 63720000 KHz @ 2160000 KHz), (N/A, 4000 mBm), (N/A)
[   22.183040] IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready
[   22.361969] usb 1-1.4: new high-speed USB device number 4 using musb-hdrc
[   22.464700] usb 1-1.4: config 1 has an invalid interface number: 8 but max is 4
[   22.464735] usb 1-1.4: config 1 has an invalid interface number: 10 but max is 4
[   22.464749] usb 1-1.4: config 1 has no interface number 1
[   22.464759] usb 1-1.4: config 1 has no interface number 4
[   22.799452] GobiNet: 2015-12-08/SWI_2.36
[   22.807353] GobiNet 1-1.4:1.8 eth1: register 'GobiNet' at usb-musb-hdrc.1.auto-1.4, GobiNet Ethernet Device, 8e:44:12:67:7b:fe
[   22.807390] RawIP mode

[    0.000000] Initializing cgroup subsys cpu
[    0.000000] Initializing cgroup subsys cpuacct
[    0.000000] Linux version 4.4.41+ (gitlab-runner@nick-NUC7i7BNHXG) (gcc version 6.2.1 20161016 (Linaro GCC 6.2-2016.11) ) #12 PREEMPT Tue May 1 17:35:09 BST 2018
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine model: TI AM335x BeagleBone Black
[    0.000000] cma: Reserved 48 MiB at 0x9d000000
[    0.000000] Memory policy: Data cache writeback
[    0.000000] On node 0 totalpages: 131072
[    0.000000] free_area_init_node: node 0, pgdat c092a90c, node_mem_map dcb61000
[    0.000000]   Normal zone: 1152 pages used for memmap
[    0.000000]   Normal zone: 0 pages reserved
[    0.000000]   Normal zone: 131072 pages, LIFO batch:31
[    0.000000] CPU: All CPU(s) started in SVC mode.
[    0.000000] AM335X ES2.1 (sgx neon )
[    0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[    0.000000] pcpu-alloc: [0] 0
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 129920
[    0.000000] Kernel command line: console=/dev/null root=PARTUUID=bf388b61-02 rw rootfstype=ext4 rootwait
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Memory: 460164K/524288K available (6603K kernel code, 266K rwdata, 2228K rodata, 260K init, 265K bss, 14972K reserved, 49152K cma-reserved, 0K highmem)
[    0.000000] Virtual kernel memory layout:
                   vector  : 0xffff0000 - 0xffff1000   (   4 kB)
                   fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
                   vmalloc : 0xe0800000 - 0xff800000   ( 496 MB)
                   lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
                   pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
                   modules : 0xbf000000 - 0xbfe00000   (  14 MB)
                     .text : 0xc0008000 - 0xc08a800c   (8833 kB)
                     .init : 0xc08a9000 - 0xc08ea000   ( 260 kB)
                     .data : 0xc08ea000 - 0xc092cad8   ( 267 kB)
                      .bss : 0xc092cad8 - 0xc096f25c   ( 266 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000] 	Build-time adjustment of leaf fanout to 32.
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[    0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[    0.000012] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[    0.000029] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[    0.000037] OMAP clocksource: timer1 at 24000000 Hz
[    0.000180] clocksource_probe: no matching clocksources found
[    0.000337] Console: colour dummy device 80x30
[    0.000373] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[    0.089267] pid_max: default: 32768 minimum: 301
[    0.089362] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.089372] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.089958] Initializing cgroup subsys io
[    0.089986] Initializing cgroup subsys memory
[    0.090017] Initializing cgroup subsys devices
[    0.090029] Initializing cgroup subsys freezer
[    0.090041] Initializing cgroup subsys perf_event
[    0.090051] Initializing cgroup subsys pids
[    0.090076] CPU: Testing write buffer coherency: ok
[    0.090432] Setting up static identity map for 0x80008200 - 0x80008260
[    0.092243] devtmpfs: initialized
[    0.102282] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[    0.115147] omap_hwmod: debugss: _wait_target_disable failed
[    0.169868] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.173330] pinctrl core: initialized pinctrl subsystem
[    0.174508] NET: Registered protocol family 16
[    0.176377] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.199258] cpuidle: using governor ladder
[    0.229248] cpuidle: using governor menu
[    0.232739] gpiochip_add: registered GPIOs 0 to 31 on device: gpio
[    0.233011] OMAP GPIO hardware version 0.1
[    0.233666] gpiochip_add: registered GPIOs 32 to 63 on device: gpio
[    0.234321] gpiochip_add: registered GPIOs 64 to 95 on device: gpio
[    0.234951] gpiochip_add: registered GPIOs 96 to 127 on device: gpio
[    0.242315] hw-breakpoint: debug architecture 0x4 unsupported.
[    0.276263] edma 49000000.edma: TI EDMA DMA engine driver
[    0.276606] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator@0[0]'
[    0.279096] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[    0.279147] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/i2c1_pins, deferring probe
[    0.279407] media: Linux media interface: v0.10
[    0.279466] Linux video capture interface: v2.00
[    0.279518] pps_core: LinuxPPS API ver. 1 registered
[    0.279524] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.279548] PTP clock support registered
[    0.279598] EDAC MC: Ver: 3.0.0
[    0.280602] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[    0.280951] Advanced Linux Sound Architecture Driver Initialized.
[    0.281955] clocksource: Switched to clocksource timer1
[    0.291008] NET: Registered protocol family 2
[    0.291681] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[    0.291726] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[    0.291764] TCP: Hash tables configured (established 4096 bind 4096)
[    0.291829] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.291845] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.292027] NET: Registered protocol family 1
[    0.292394] RPC: Registered named UNIX socket transport module.
[    0.292407] RPC: Registered udp transport module.
[    0.292412] RPC: Registered tcp transport module.
[    0.292418] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.292446] PCI: CLS 0 bytes, default 64
[    0.293273] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[    0.294958] futex hash table entries: 256 (order: -1, 3072 bytes)
[    0.301406] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.302197] NFS: Registering the id_resolver key type
[    0.302261] Key type id_resolver registered
[    0.302268] Key type id_legacy registered
[    0.302327] ntfs: driver 2.1.32 [Flags: R/O].
[    0.303993] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[    0.304019] io scheduler noop registered
[    0.304030] io scheduler deadline registered
[    0.304058] io scheduler cfq registered (default)
[    0.305280] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[    0.307975] pwm-backlight backlight: GPIO lookup for consumer enable
[    0.307997] pwm-backlight backlight: using device tree for GPIO lookup
[    0.308010] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/backlight[0]'
[    0.308019] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/backlight[0]'
[    0.308027] pwm-backlight backlight: using lookup tables for GPIO lookup
[    0.308036] pwm-backlight backlight: lookup for GPIO enable failed
[    0.308057] backlight supply power not found, using dummy regulator
[    0.358758] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[    0.362409] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[    0.363472] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 159, base_baud = 3000000) is a 8250
[    0.364433] 48024000.serial: ttyS2 at MMIO 0x48024000 (irq = 160, base_baud = 3000000) is a 8250
[    0.365337] 481a8000.serial: ttyS4 at MMIO 0x481a8000 (irq = 161, base_baud = 3000000) is a 8250
[    0.366973] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[    0.367101] [drm] Initialized drm 1.1.0 20060810
[    0.378059] brd: module loaded
[    0.383551] loop: module loaded
[    0.387049] libphy: Fixed MDIO Bus: probed
[    0.452020] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[    0.452041] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[    0.452908] libphy: 4a101000.mdio: probed
[    0.452932] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720
[    0.453528] cpsw 4a100000.ethernet: Detected MACID = 2c:6b:7d:5a:3f:86
[    0.453645] cpsw 4a100000.ethernet: cpts: overflow check period 850
[    0.454892] mousedev: PS/2 mouse device common for all mice
[    0.455385] i2c /dev entries driver
[    0.456445] cpuidle: enable-method property 'ti,am3352' found operations
[    0.457044] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[    0.457059] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[    0.457085] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp/mmc@48060000[0]' - status (0)
[    0.457159] omap_hsmmc 48060000.mmc: Got CD GPIO
[    0.457171] omap_hsmmc 48060000.mmc: GPIO lookup for consumer wp
[    0.457179] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[    0.457188] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@48060000[0]'
[    0.457197] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@48060000[0]'
[    0.457205] omap_hsmmc 48060000.mmc: using lookup tables for GPIO lookup
[    0.457214] omap_hsmmc 48060000.mmc: lookup for GPIO wp failed
[    0.492498] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer cd
[    0.492517] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
[    0.492528] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp/mmc@481d8000[0]'
[    0.492620] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp/mmc@481d8000[0]'
[    0.492630] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
[    0.492639] omap_hsmmc 481d8000.mmc: lookup for GPIO cd failed
[    0.492650] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer wp
[    0.492657] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
[    0.492665] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@481d8000[0]'
[    0.492672] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@481d8000[0]'
[    0.492680] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
[    0.492687] omap_hsmmc 481d8000.mmc: lookup for GPIO wp failed
[    0.532540] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@2[0]' - status (0)
[    0.532759] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@3[0]' - status (0)
[    0.532876] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@4[0]' - status (0)
[    0.532980] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@5[0]' - status (0)
[    0.533408] ledtrig-cpu: registered to indicate activity on CPUs
[    0.537190] NET: Registered protocol family 10
[    0.540443] sit: IPv6 over IPv4 tunneling driver
[    0.541137] NET: Registered protocol family 17
[    0.541420] Key type dns_resolver registered
[    0.541643] omap_voltage_late_init: Voltage driver support not added
[    0.569005] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[    0.569257] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[    0.569294] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[    0.570263] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 100 kHz
[    0.572354] of_get_named_gpiod_flags: parsed 'gpios' property of node '/wakeup_keys@0/test@0[0]' - status (0)
[    0.572392] of_get_named_gpiod_flags: parsed 'gpios' property of node '/wakeup_keys@0/test@1[0]' - status (0)
[    0.572791] input: wakeup_keys@0 as /devices/platform/wakeup_keys@0/input/input0
[    0.573242] hctosys: unable to open rtc device (rtc0)
[    0.576183] mmc1: MAN_BKOPS_EN bit is not set
[    0.576711] ALSA device list:
[    0.576726]   No soundcards found.
[    0.576853] Warning: unable to open an initial console.
[    0.577048] Waiting for root device PARTUUID=bf388b61-02...
[    0.579989] mmc1: new high speed MMC card at address 0001
[    0.580673] mmcblk0: mmc1:0001 MMC04G 3.52 GiB
[    0.580906] mmcblk0boot0: mmc1:0001 MMC04G partition 1 16.0 MiB
[    0.581124] mmcblk0boot1: mmc1:0001 MMC04G partition 2 16.0 MiB
[    0.583236]  mmcblk0: p1 p2
[    0.707650] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    0.707726] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    0.715903] devtmpfs: mounted
[    0.716199] Freeing unused kernel memory: 260K (c08a9000 - c08ea000)
[    0.716206] This architecture does not have kernel memory protection.
[    1.033979] systemd[1]: System time before build time, advancing clock.
[    1.105509] random: systemd: uninitialized urandom read (16 bytes read, 15 bits of entropy available)
[    1.113643] random: systemd: uninitialized urandom read (16 bytes read, 15 bits of entropy available)
[    1.140635] systemd[1]: systemd 230 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[    1.141949] systemd[1]: Detected architecture arm.
[    1.166363] systemd[1]: Set hostname to <scada>.
[    1.247669] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 19 bits of entropy available)
[    1.268044] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 19 bits of entropy available)
[    1.268515] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 19 bits of entropy available)
[    1.293226] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 19 bits of entropy available)
[    1.301404] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
[    1.395013] random: systemd: uninitialized urandom read (16 bytes read, 24 bits of entropy available)
[    1.395410] random: systemd: uninitialized urandom read (16 bytes read, 24 bits of entropy available)
[    1.397297] random: systemd: uninitialized urandom read (16 bytes read, 24 bits of entropy available)
[    1.461854] systemd[1]: [/lib/systemd/system/gadget-init.service:15] Unknown lvalue 'ExecStopPre' in section 'Service'
[    1.724601] systemd[1]: sysinit.target: Found ordering cycle on sysinit.target/start
[    1.724654] systemd[1]: sysinit.target: Found dependency on alignment.service/start
[    1.724684] systemd[1]: sysinit.target: Found dependency on sysinit.target/start
[    1.724706] systemd[1]: sysinit.target: Breaking ordering cycle by deleting job alignment.service/start
[    1.724731] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with sysinit.target/start
[    1.730781] systemd[1]: Listening on Syslog Socket.
[    1.731516] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[    1.732151] systemd[1]: Listening on Journal Socket.
[    1.732571] systemd[1]: Listening on udev Kernel Socket.
[    1.732920] systemd[1]: Listening on Journal Socket (/dev/log).
[    1.733237] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[    1.733576] systemd[1]: Listening on udev Control Socket.
[    1.735671] systemd[1]: Created slice User and Session Slice.
[    1.736167] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[    1.736337] systemd[1]: Reached target Paths.
[    1.736467] systemd[1]: Reached target Swap.
[    1.736635] systemd[1]: Reached target Remote File Systems.
[    1.763548] systemd[1]: Listening on Network Service Netlink Socket.
[    1.764931] systemd[1]: Created slice System Slice.
[    1.766337] systemd[1]: Created slice system-serial\x2dgetty.slice.
[    1.770616] systemd[1]: Starting Journal Service...
[    1.777790] systemd[1]: Mounting Debug File System...
[    1.814501] systemd[1]: Mounting Temporary Directory...
[    1.845636] systemd[1]: Starting Create Static Device Nodes in /dev...
[    1.850090] systemd[1]: Starting Setup Virtual Console...
[    1.850403] systemd[1]: Reached target Slices.
[    1.917272] systemd[1]: Starting Load Kernel Modules...
[    1.921869] systemd[1]: Starting Remount Root and Kernel File Systems...
[    2.001811] systemd[1]: Created slice system-getty.slice.
[    2.051759] systemd[1]: Mounting POSIX Message Queue File System...
[    2.144107] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[    2.171274] systemd[1]: Mounted Debug File System.
[    2.171606] systemd[1]: Mounted POSIX Message Queue File System.
[    2.171792] systemd[1]: Mounted Temporary Directory.
[    2.185357] systemd[1]: Started Create Static Device Nodes in /dev.
[    2.186882] systemd[1]: Started Setup Virtual Console.
[    2.188284] systemd[1]: Started Remount Root and Kernel File Systems.
[    2.226325] systemd[1]: Starting udev Coldplug all Devices...
[    2.226720] systemd[1]: Reached target Local File Systems (Pre).
[    2.250825] systemd[1]: Mounting /media/ram...
[    2.297766] usbcore: registered new interface driver usbfs
[    2.297869] usbcore: registered new interface driver hub
[    2.314942] systemd[1]: Mounting /var/volatile...
[    2.328849] usbcore: registered new device driver usb
[    2.350033] systemd[1]: Starting udev Kernel Device Manager...
[    2.408344] systemd[1]: Mounted /media/ram.
[    2.409204] systemd[1]: Started Journal Service.
[    2.439849] usbcore: registered new interface driver ath9k_htc
[    2.490725] ip_tables: (C) 2000-2006 Netfilter Core Team
[    2.511481] nf_conntrack version 0.5.0 (7962 buckets, 31848 max)
[    2.702404] systemd-journald[86]: Received request to flush runtime journal from PID 1
[    3.269045] cfg80211: World regulatory domain updated:
[    3.269081] cfg80211:  DFS Master region: unset
[    3.269091] cfg80211:   (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)
[    3.269103] cfg80211:   (2402000 KHz - 2472000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)
[    3.269115] cfg80211:   (2457000 KHz - 2482000 KHz @ 20000 KHz, 92000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[    3.269123] cfg80211:   (2474000 KHz - 2494000 KHz @ 20000 KHz), (N/A, 2000 mBm), (N/A)
[    3.269132] cfg80211:   (5170000 KHz - 5250000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[    3.269141] cfg80211:   (5250000 KHz - 5330000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (0 s)
[    3.269149] cfg80211:   (5490000 KHz - 5730000 KHz @ 160000 KHz), (N/A, 2000 mBm), (0 s)
[    3.269157] cfg80211:   (5735000 KHz - 5835000 KHz @ 80000 KHz), (N/A, 2000 mBm), (N/A)
[    3.269164] cfg80211:   (57240000 KHz - 63720000 KHz @ 2160000 KHz), (N/A, 0 mBm), (N/A)
[    4.366021] omap_rtc 44e3e000.rtc: already running
[    4.404741] rtc rtc0: 44e3e000.rtc: dev (254:0)
[    4.404795] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[    4.450927] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    4.537663] TI-am335x-tsc TI-am335x-tsc: ti,charge-delay not specified
[    4.538001] input: ti-tsc as /devices/platform/ocp/44e0d000.tscadc/TI-am335x-tsc/input/input1
[    4.942234] CAN device driver interface
[    5.045845] c_can_platform 481cc000.can: c_can_platform device registered (regs=fa1cc000, irq=167)
[    5.400960] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[    5.510335] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[    5.559997]  remoteproc0: wkup_m3 is available
[    5.560024]  remoteproc0: Note: remoteproc is still under development and considered experimental.
[    5.560032]  remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[    5.583632] ti-pruss 4a300000.pruss: creating PRU cores and other child platform devices
[    5.584738] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[    5.585233] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[    5.634790]  remoteproc1: 4a334000.pru0 is available
[    5.634818]  remoteproc1: Note: remoteproc is still under development and considered experimental.
[    5.634825]  remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[    5.641422]  remoteproc1: registered virtio0 (type 7)
[    5.660454] pru-rproc 4a334000.pru0: PRU rproc node /ocp/pruss@4a300000/pru0@4a334000 probed successfully
[    5.660983]  remoteproc2: 4a338000.pru1 is available
[    5.661000]  remoteproc2: Note: remoteproc is still under development and considered experimental.
[    5.661008]  remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[    5.666622]  remoteproc2: registered virtio1 (type 7)
[    5.666724] pru-rproc 4a338000.pru1: PRU rproc node /ocp/pruss@4a300000/pru1@4a338000 probed successfully
[    5.880938]  remoteproc0: powering up wkup_m3
[    5.883519] PM: bootloader does not support rtc-only!
[    5.898570]  remoteproc0: Booting fw image am335x-pm-firmware.elf, size 224344
[    5.898852]  remoteproc0: remote processor wkup_m3 is now up
[    5.898885] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[    7.066102] net eth0: initializing cpsw version 1.12 (0)
[    7.066154] net eth0: initialized cpsw ale version 1.4
[    7.066163] net eth0: ALE Table size 1024
[    7.068625] net eth0: phy found : id is : 0x7c0f1
[    7.068706] libphy: PHY 4a101000.mdio:01 not found
[    7.068717] net eth0: phy "4a101000.mdio:01" not found on slave 1, err -19
[    7.137038] Bluetooth: Core ver 2.21
[    7.137148] NET: Registered protocol family 31
[    7.137157] Bluetooth: HCI device and connection manager initialized
[    7.137180] Bluetooth: HCI socket layer initialized
[    7.137194] Bluetooth: L2CAP socket layer initialized
[    7.137224] Bluetooth: SCO socket layer initialized
[    7.253726] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[    9.763622] NET: Registered protocol family 15
[    9.962597] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[   10.576830] Initializing XFRM netlink socket
[   11.102888] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[   11.103013] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[   11.254237] random: nonblocking pool is initialized
[   12.854057] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517
[   12.854350] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517
[   12.865693] musb-hdrc musb-hdrc.1.auto: musb_init_controller failed with status -517
[   12.866003] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517
[   12.866152] musb-hdrc musb-hdrc.1.auto: musb_init_controller failed with status -517
[   12.874170] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer reset
[   12.874200] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lookup
[   12.874216] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[   12.874226] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[   12.874234] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO lookup
[   12.874244] am335x-phy-driver 47401300.usb-phy: lookup for GPIO reset failed
[   12.874254] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer vbus-detect
[   12.874262] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lookup
[   12.874271] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[   12.874279] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[   12.874287] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO lookup
[   12.874295] am335x-phy-driver 47401300.usb-phy: lookup for GPIO vbus-detect failed
[   12.874359] 47401300.usb-phy supply vcc not found, using dummy regulator
[   12.978393] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer reset
[   12.978427] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lookup
[   12.978444] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[   12.978453] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[   12.978462] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO lookup
[   12.978472] am335x-phy-driver 47401b00.usb-phy: lookup for GPIO reset failed
[   12.978482] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer vbus-detect
[   12.978490] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lookup
[   12.978499] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[   12.978507] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[   12.978515] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO lookup
[   12.978524] am335x-phy-driver 47401b00.usb-phy: lookup for GPIO vbus-detect failed
[   12.978590] 47401b00.usb-phy supply vcc not found, using dummy regulator
[   13.025427] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[   13.025455] musb-hdrc: MHDRC RTL version 2.0
[   13.025464] musb-hdrc: setup fifo_mode 4
[   13.025482] musb-hdrc: 28/31 max ep, 16384/16384 memory
[   13.047476] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[   13.047505] musb-hdrc: MHDRC RTL version 2.0
[   13.047513] musb-hdrc: setup fifo_mode 4
[   13.047529] musb-hdrc: 28/31 max ep, 16384/16384 memory
[   13.047656] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[   13.047698] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 1
[   13.107434] hub 1-0:1.0: USB hub found
[   13.107498] hub 1-0:1.0: 1 port detected
[   14.385318]  remoteproc1: powering up 4a334000.pru0
[   14.385821]  remoteproc1: Booting fw image am335x-pru0-fw, size 75688
[   14.386008] ti-pruss 4a300000.pruss: configured system_events = 0x0000000000030000 intr_channels = 0x00000005 host_intr = 0x00000005
[   14.397776]  remoteproc1: remote processor 4a334000.pru0 is now up
[   14.398099] virtio_rpmsg_bus virtio0: creating channel rpmsg-pru addr 0x1e
[   14.401603] virtio_rpmsg_bus virtio0: rpmsg host is online
[   14.401902]  remoteproc2: powering up 4a338000.pru1
[   14.403103]  remoteproc2: Booting fw image am335x-pru1-fw, size 75688
[   14.403295] ti-pruss 4a300000.pruss: configured system_events = 0x00000000000c0000 intr_channels = 0x0000000a host_intr = 0x0000000a
[   14.415108]  remoteproc2: remote processor 4a338000.pru1 is now up
[   14.415442] virtio_rpmsg_bus virtio1: creating channel rpmsg-pru addr 0x1f
[   14.415688] virtio_rpmsg_bus virtio1: rpmsg host is online
[   14.671400] rpmsg_pru rpmsg0: new rpmsg_pru device: /dev/rpmsg_pru30
[   14.671677] rpmsg_pru rpmsg1: new rpmsg_pru device: /dev/rpmsg_pru31

Regards

  • this is the SDK version : 04_00_00_04
  • Nick,

    Nick King said:
    now sometimes the usb drivers fail to boot up

    Both logs show the USB drivers are loaded correctly during kernel booting up. Do you mean the issue is that the USB device is not detected?

    Nick King said:
    it shows some strange error in the fail attempt : [   12.906464] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517

    This log message is not an error, it only tells that when kernel loading the MUSB driver, the CPPI41 DMA driver is not loaded yet, and kernel will run the MUSB driver init later when the CPPI41 driver is loaded.

    I see the successful log shows a 4-port USB hub is enumerated, but not in the failure log. Is this an external hub or on-board hub?

    Please post the USB portion of the schematics of your board.

  • Thanks a lot bin liu

    this is a custom board which is based on BBB USB hub is on board hub

    Yes i mean after reboot i do not see any USB devices are detected i wait for more than 5 minutes still usb devices do not detect(logs dmesg_usb_fails_to_boot.txt). and if i reboot again the second time on the same board this time i see USB device is detected. and usb works fine.

    please see the schematics of usb hub portion

    Regards

  • Nick,

    In the failure case, please run the following command on your board to dump two usb registers.

    # grep -i 'devctl\|power' /sys/kernel/debug/musb-hdrc.1.auto/regdump
  • thanks bin liu

    1. so you think the schematics of usb hub is correct?
    2. i will try this commands give me some time.

    Regards
  • Nick,

    The connections on AM335x side seem to be fine, so we need to check the AM335x USB controller state.
    If the state is not correct, we need to debug why.
    If the state is correct, that means the hub design has issues, you would have to get support from the hub vendor.
  • hi liu

    today i tried again 15 times all 14 times it booted up successfully  and at the 15th attempt it fails.

    on failed attempt bellow is the value of the regdump

    -------------

    root@evm:/# grep -i 'devctl\|power' /sys/kernel/debug/musb-hdrc.1.auto/regdump

    Power : e0
    DevCtl : 89

    ------------

    on success full usb boot bellow is the value

    --------------

    root@scada:/# grep -i 'devctl\|power' /sys/kernel/debug/musb-hdrc.1.auto/regdump

    Power : f0
    DevCtl : 5d

    ----------------

    Regards

  • Nick,

    The register dump in the failure case shows the musb controller is NOT in the proper state. Please test the same using the latest Processor SDK v4.3 to see if the issue still happens. If so, I will provide instructions to get kernel debug log to understand why it fails.

    Testing on SDK v4.3 is easier than debugging the problem, so we want to go to the easy route first.

  • Thanks Bin Liu

    1. So is it software issue or hardware issue so i can atleast make a decision of either switch to lastest sdk or debug hardware.
  • Nick,

    I am unable to tell if it is hw or sw issue at this moment. Obviously it is hw timing causes the controller not function correctly.
    I could check the kernel to see if any patch since SDK 4.0 is related, but I am current preparing for an event tomorrow. So you could either test SDK v4.3 now or wait until this Wednesday when I will check the latest kernel patches.
  • Nick,

    If you haven't started testing the latest SDK kernel, please apply the following debug patch in your current SDK 4.0 kernel, and attach the kernel dmesg log when the issue happens.

    diff --git a/drivers/usb/musb/musb_core.c b/drivers/usb/musb/musb_core.c
    index a50bf6758601..13d78be3b3ee 100644
    --- a/drivers/usb/musb/musb_core.c
    +++ b/drivers/usb/musb/musb_core.c
    @@ -575,6 +575,9 @@ static irqreturn_t musb_stage0_irq(struct musb *musb, u8 int_usb,
            irqreturn_t handled = IRQ_NONE;
     
            musb_dbg(musb, "<== DevCtl=%02x, int_usb=0x%x", devctl, int_usb);
    +       dev_info(musb->controller, "<== DevCtl=%02x, int_usb=0x%x, state %s\n",
    +                       devctl, int_usb,
    +                       usb_otg_state_string(musb->xceiv->otg->state));
     
            /* in host mode, the peripheral may issue remote wakeup.
             * in peripheral mode, the host may resume the link.
    
  • Nick,

    I haven’t heard back from you, I’m assuming you were able to resolve your issue. If not, just post a reply below (or create a new thread if the thread has locked due to time-out). thanks.
  • hi liu sorry for the delay now i am using the latest TI SDK now i tried to reboot the board 25 times i did not see this issue again. but i have other issue with usb
  • Nick,

    Glad to hear this issue is gone in the latest kernel.
    Please open an new thread for the new usb issue if you need help.