This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: Kernel boot issue

Part Number: AM5728
Other Parts Discussed in Thread: DRA752, TPD12S015, TMP102

Tool/software: Linux

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.14.32-gdc3e450ded (oe-user@oe-host) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #5 SMP PREEMPT Sat May 5 06:18:35 PDT 2018
[    0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[    0.000000] CPU: div instructions available: patching division code
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[    0.000000] OF: fdt: Machine model: TI AM572x EVM Rev A3
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[    0.000000] OF: reserved mem: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
[    0.000000] OF: reserved mem: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
[    0.000000] OF: reserved mem: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created CMA memory pool at 0x000000009f000000, size 8 MiB
[    0.000000] OF: reserved mem: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[    0.000000] cma: Reserved 24 MiB at 0x00000000fe400000
[    0.000000] OMAP4: Map 0x00000000ffd00000 to fe600000 for dram barrier
[    0.000000] DRA752 ES2.0
[    0.000000] random: fast init done
[    0.000000] percpu: Embedded 15 pages/cpu @eed30000 s31308 r8192 d21940 u61440
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 471616
[    0.000000] Kernel command line: console=ttyO2,115200n8 root=PARTUUID=621419fc-02 rw rootfstype=ext4 rootwait
[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Memory: 1671564K/1893376K available (8192K kernel code, 346K rwdata, 2560K rodata, 2048K init, 298K bss, 33396K reserved, 188416K cma-reserved, 1278976K highmem)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
[    0.000000]     vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc0a00000   (10208 kB)
[    0.000000]       .init : 0xc0e00000 - 0xc1000000   (2048 kB)
[    0.000000]       .data : 0xc1000000 - 0xc1056828   ( 347 kB)
[    0.000000]        .bss : 0xc1058000 - 0xc10a2bfc   ( 299 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Tasks RCU enabled.
[    0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[    0.000000] OMAP clockevent source: timer1 at 32786 Hz
[    0.000000] arch_timer: cp15 timer(s) running at 6.14MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[    0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[    0.000017] Switching to timer-based delay loop, resolution 162ns
[    0.000346] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[    0.000355] OMAP clocksource: 32k_counter at 32768 Hz
[    0.000809] Console: colour dummy device 80x30
[    0.000827] WARNING: Your 'console=ttyO2' has been replaced by 'ttyS2'
[    0.000834] This ensures that you still see kernel messages. Please
[    0.000841] update your kernel commandline.
[    0.000863] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[    0.000879] pid_max: default: 32768 minimum: 301
[    0.000999] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.001013] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.001533] CPU: Testing write buffer coherency: ok
[    0.001747] /cpus/cpu@0 missing clock-frequency property
[    0.001765] /cpus/cpu@1 missing clock-frequency property
[    0.001777] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.039869] Setting up static identity map for 0x80200000 - 0x80200060
[    0.059881] Hierarchical SRCU implementation.
[    0.080068] EFI services will not be available.
[    0.099943] smp: Bringing up secondary CPUs ...
[    0.170284] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.170376] smp: Brought up 1 node, 2 CPUs
[    0.170391] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[    0.170399] CPU: All CPU(s) started in HYP mode.
[    0.170406] CPU: Virtualization extensions available.
[    0.170831] devtmpfs: initialized
[    0.189341] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[    0.189533] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.189550] futex hash table entries: 512 (order: 3, 32768 bytes)
[    0.193364] pinctrl core: initialized pinctrl subsystem
[    0.193812] DMI not present or invalid.
[    0.194064] NET: Registered protocol family 16
[    0.195118] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.196043] omap_hwmod: l3_main_2 using broken dt data from ocp
[    0.304070] omap_hwmod: dcan1: _wait_target_disable failed
[    0.402974] cpuidle: using governor ladder
[    0.403005] cpuidle: using governor menu
[    0.411036] OMAP GPIO hardware version 0.1
[    0.440693] No ATAGs?
[    0.440765] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[    0.440779] hw-breakpoint: maximum watchpoint size is 8 bytes.
[    0.441153] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[    0.441164] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[    0.441680] OMAP DMA hardware revision 0.0
[    0.456597] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[    0.457916] edma 43300000.edma: memcpy is disabled
[    0.461182] edma 43300000.edma: TI EDMA DMA engine driver
[    0.464885] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[    0.465078] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[    0.465325] omap-iommu 58882000.mmu: 58882000.mmu registered
[    0.465568] omap-iommu 55082000.mmu: 55082000.mmu registered
[    0.465922] omap-iommu 41501000.mmu: 41501000.mmu registered
[    0.466126] omap-iommu 41502000.mmu: 41502000.mmu registered
[    0.466373] iommu: Adding device 58820000.ipu to group 1
[    0.466452] iommu: Adding device 55020000.ipu to group 2
[    0.466593] iommu: Adding device 40800000.dsp to group 0
[    0.466833] iommu: Adding device 41000000.dsp to group 3
[    0.469210] palmas 0-0058: Irq flag is 0x00000008
[    1.062097] random: crng init done
[   64.115711] irq 178: nobody cared (try booting with the "irqpoll" option)
[   64.115725] CPU: 0 PID: 27 Comm: irq/178-palmas Not tainted 4.14.32-gdc3e450ded #5
[   64.115734] Hardware name: Generic DRA74X (Flattened Device Tree)
[   64.115741] Backtrace:
[   64.115763] [<c020b5fc>] (dump_backtrace) from [<c020b8e0>] (show_stack+0x18/0x1c)
[   64.115775]  r7:000000b2 r6:20000193 r5:00000000 r4:c105366c
[   64.115790] [<c020b8c8>] (show_stack) from [<c091c8e8>] (dump_stack+0x90/0xa4)
[   64.115806] [<c091c858>] (dump_stack) from [<c0281ae0>] (__report_bad_irq+0x30/0xd4)
[   64.115817]  r7:000000b2 r6:eea50210 r5:00000000 r4:eeb5f200
[   64.115830] [<c0281ab0>] (__report_bad_irq) from [<c0281ed4>] (note_interrupt+0x270/0x2bc)
[   64.115841]  r9:20000193 r8:00000001 r7:000000b2 r6:eea50210 r5:00000000 r4:eeb5f200
[   64.115855] [<c0281c64>] (note_interrupt) from [<c027f104>] (handle_irq_event_percpu+0x54/0x60)
[   64.115865]  r10:00000000 r9:20000193 r8:00000001 r7:eea50268 r6:eea50210 r5:eeb5f200
[   64.115872]  r4:00000002 r3:00000000
[   64.115885] [<c027f0b0>] (handle_irq_event_percpu) from [<c027f150>] (handle_irq_event+0x40/0x64)
[   64.115893]  r5:eeb5f264 r4:eeb5f200
[   64.115905] [<c027f110>] (handle_irq_event) from [<c02828f8>] (handle_level_irq+0xb4/0x134)
[   64.115914]  r7:eea50268 r6:eea50210 r5:eeb5f264 r4:eeb5f200
[   64.115926] [<c0282844>] (handle_level_irq) from [<c027e238>] (generic_handle_irq+0x2c/0x3c)
[   64.115934]  r5:eea50264 r4:00000000
[   64.115949] [<c027e20c>] (generic_handle_irq) from [<c052e1d8>] (omap_gpio_irq_handler+0x108/0x15c)
[   64.115962] [<c052e0d0>] (omap_gpio_irq_handler) from [<c027efe8>] (__handle_irq_event_percpu+0x6c/0x134)
[   64.115973]  r10:c105508d r9:eea35500 r8:00000025 r7:eeb7fdec r6:00000000 r5:eea35500
[   64.115980]  r4:eea378c0
[   64.115992] [<c027ef7c>] (__handle_irq_event_percpu) from [<c027f0d4>] (handle_irq_event_percpu+0x24/0x60)
[   64.116002]  r10:c02801f0 r9:eeb7e000 r8:ee808000 r7:00000000 r6:c1022048 r5:eea35500
[   64.116009]  r4:eea35500
[   64.116020] [<c027f0b0>] (handle_irq_event_percpu) from [<c027f150>] (handle_irq_event+0x40/0x64)
[   64.116028]  r5:eea35564 r4:eea35500
[   64.116040] [<c027f110>] (handle_irq_event) from [<c0282a24>] (handle_fasteoi_irq+0xac/0x160)
[   64.116049]  r7:00000000 r6:c1022048 r5:eea35564 r4:eea35500
[   64.116060] [<c0282978>] (handle_fasteoi_irq) from [<c027e238>] (generic_handle_irq+0x2c/0x3c)
[   64.116069]  r7:00000000 r6:00000000 r5:00000025 r4:c0e63afc
[   64.116080] [<c027e20c>] (generic_handle_irq) from [<c027e7c0>] (__handle_domain_irq+0x64/0xbc)
[   64.116091] [<c027e75c>] (__handle_domain_irq) from [<c0201474>] (gic_handle_irq+0x44/0x80)
[   64.116101]  r9:eeb7e000 r8:fa213000 r7:fa212000 r6:eeb7fea8 r5:fa21200c r4:c1004000
[   64.116112] [<c0201430>] (gic_handle_irq) from [<c020c4b8>] (__irq_svc+0x58/0x8c)
[   64.116120] Exception stack(0xeeb7fea8 to 0xeeb7fef0)
[   64.116130] fea0:                   eeb5f264 a0000093 00000000 c052dfd4 eeb5f200 eeb5f264
[   64.116140] fec0: eeb60880 eeb5f214 eeb5f200 eeb60880 c02801f0 eeb7ff14 eeb7fef8 eeb7fef8
[   64.116149] fee0: c0280110 c028011c a0000013 ffffffff
[   64.116158]  r9:eeb7e000 r8:eeb5f200 r7:eeb7fedc r6:ffffffff r5:a0000013 r4:c028011c
[   64.116171] [<c028008c>] (irq_finalize_oneshot.part.1) from [<c0280244>] (irq_thread_fn+0x54/0x5c)
[   64.116180]  r7:00000001 r6:00000000 r5:eeb5f200 r4:eeb60880
[   64.116192] [<c02801f0>] (irq_thread_fn) from [<c0280514>] (irq_thread+0x14c/0x204)
[   64.116200]  r7:00000001 r6:00000000 r5:ffffe000 r4:eeb608a4
[   64.116213] [<c02803c8>] (irq_thread) from [<c0248738>] (kthread+0x164/0x16c)
[   64.116223]  r10:ee87f938 r9:c02803c8 r8:eeb60880 r7:eeb7e000 r6:00000000 r5:eeb608c0
[   64.116230]  r4:ee9de200
[   64.116242] [<c02485d4>] (kthread) from [<c0207d98>] (ret_from_fork+0x14/0x3c)
[   64.116252]  r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c02485d4
[   64.116259]  r4:eeb608c0
[   64.116265] handlers:
[   64.116274] [<c027f1c8>] irq_default_primary_handler threaded [<c0669070>] regmap_irq_thread
[   64.116295] Disabling IRQ #178
[   64.117074] palmas 0-0058: Muxing GPIO 2f, PWM 0, LED 0
[   64.118647] SMPS12: supplied by regulator-dummy
[   64.120354] SMPS3: supplied by regulator-dummy
[   64.121883] SMPS45: supplied by regulator-dummy
[   64.123696] SMPS6: supplied by regulator-dummy
[   64.125110] SMPS7: supplied by regulator-dummy
[   64.126501] SMPS8: supplied by regulator-dummy
[   64.126832] smps8: Bringing 1060000uV into 1800000-1800000uV
[   64.127135] smps8: failed to apply 1800000-1800000uV constraint(-22)
[   64.127149] palmas-pmic 48070000.i2c:tps659038@58:tps659038_pmic: failed to register 48070000.i2c:tps659038@58:tps659038_pmic regulator
[   64.128340] palmas-pmic: probe of 48070000.i2c:tps659038@58:tps659038_pmic failed with error -22
[   64.129721] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[   64.130236] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[   64.130696] omap_i2c 4807c000.i2c: bus 4 rev0.12 at 400 kHz
[   64.130905] media: Linux media interface: v0.10
[   64.130945] Linux video capture interface: v2.00
[   64.131023] pps_core: LinuxPPS API ver. 1 registered
[   64.131032] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[   64.131051] PTP clock support registered
[   64.131078] EDAC MC: Ver: 3.0.0
 ? mmc_init:  [CCTV]
[   64.131328] dmi: Firmware registration failed.
[   64.131706] omap-mailbox 4883c000.mailbox: omap mailbox rev 0x400
[   64.131980] omap-mailbox 4883e000.mailbox: omap mailbox rev 0x400
[   64.132255] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[   64.132520] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[   64.132842] Advanced Linux Sound Architecture Driver Initialized.
[   64.133515] clocksource: Switched to clocksource arch_sys_counter
[   64.141206] NET: Registered protocol family 2
[   64.141719] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[   64.141783] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[   64.141909] TCP: Hash tables configured (established 8192 bind 8192)
[   64.141978] UDP hash table entries: 512 (order: 2, 16384 bytes)
[   64.142012] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[   64.142136] NET: Registered protocol family 1
[   64.142423] RPC: Registered named UNIX socket transport module.
[   64.142433] RPC: Registered udp transport module.
[   64.142441] RPC: Registered tcp transport module.
[   64.142449] RPC: Registered tcp NFSv4.1 backchannel transport module.
[   64.143344] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[   64.143581] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[   64.144590] workingset: timestamp_bits=14 max_order=19 bucket_order=5
[   64.148530] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[   64.149022] NFS: Registering the id_resolver key type
[   64.149043] Key type id_resolver registered
[   64.149052] Key type id_legacy registered
[   64.149089] ntfs: driver 2.1.32 [Flags: R/O].
[   64.150350] bounce: pool size: 64 pages
[   64.150394] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[   64.150404] io scheduler noop registered
[   64.150412] io scheduler deadline registered
[   64.150564] io scheduler cfq registered (default)
[   64.150574] io scheduler mq-deadline registered
[   64.150582] io scheduler kyber registered
[   64.155396] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[   64.158590] dra7-pcie 51000000.pcie: Linked as a consumer to phy-4a094000.pciephy.1
[   64.158821] dra7-pcie 51000000.pcie: WA for Errata i870 not appplied. Update DT
[   64.158921] OF: PCI: host bridge /ocp/axi@0/pcie@51000000 ranges:
[   64.158934] OF: PCI:   No bus range found for /ocp/axi@0/pcie@51000000, using [bus 00-ff]
[   64.158968] OF: PCI:    IO 0x20003000..0x20012fff -> 0x00000000
[   64.158990] OF: PCI:   MEM 0x20013000..0x2fffffff -> 0x20013000
[   65.153656] dra7-pcie 51000000.pcie: phy link never came up
[   65.153789] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[   65.153803] pci_bus 0000:00: root bus resource [bus 00-ff]
[   65.153815] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
[   65.153826] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[   65.154135] PCI: bus0: Fast back to back transfers disabled
[   65.154222] PCI: bus1: Fast back to back transfers enabled
[   65.154260] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff 64bit]
[   65.154279] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[   65.154562] pcieport 0000:00:00.0: Signaling PME with IRQ 181
[   65.154685] pcieport 0000:00:00.0: AER enabled with IRQ 181
[   65.155674] pwm-backlight backlight: backlight supply power not found, using dummy regulator
[   65.199511] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[   65.202036] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 45, base_baud = 3000000) is a 8250
[   66.645997] console [ttyS2] enabled
[   66.650244] 48422000.serial: ttyS7 at MMIO 0x48422000 (irq = 46, base_baud = 3000000) is a 8250
[   66.660960] omap_rng 48090000.rng: Random Number Generator ver. 20
[   66.668706] omapdss_dss 58000000.dss: master bind failed: -517
[   66.675412] tpd12s015 encoder: failed to find video source
[   66.681622] connector-hdmi connector: failed to find video source
[   66.688102] panel-dpi display: display supply vcc not found, using dummy regulator
[   66.695879] panel-dpi display: failed to find video source
[   66.709050] brd: module loaded
[   66.717480] loop: module loaded
[   66.747233] libphy: Fixed MDIO Bus: probed
[   66.813541] davinci_mdio 48485000.mdio: davinci mdio revision 1.6, bus freq 1000000
[   66.821233] libphy: 48485000.mdio: probed
[   66.829224] davinci_mdio: probe of 48485000.mdio failed with error -5
[   66.836226] cpsw 48484000.ethernet: Detected MACID = 7c:38:66:95:6e:fa
[   66.842834] cpsw 48484000.ethernet: initialized cpsw ale version 1.4
[   66.849241] cpsw 48484000.ethernet: ALE Table size 1024
[   66.854573] cpsw 48484000.ethernet: cpts: overflow check period 500 (jiffies)
[   66.862434] cpsw 48484000.ethernet: cpsw: Detected MACID = 7c:38:66:95:6e:fb
[   66.870683] i2c /dev entries driver
[   66.875117] IR NEC protocol handler initialized
[   66.879669] IR RC5(x/sz) protocol handler initialized
[   66.884763] IR RC6 protocol handler initialized
[   66.889314] IR JVC protocol handler initialized
[   66.893921] IR Sony protocol handler initialized
[   66.898559] IR SANYO protocol handler initialized
[   66.903283] IR Sharp protocol handler initialized
[   66.908026] IR MCE Keyboard/mouse protocol handler initialized
[   66.913917] IR XMP protocol handler initialized
[   66.920745] gpio-fan gpio_fan: GPIO fan initialized
[   66.926304] tmp102 0-0048: error reading config register
[   66.931766] tmp102: probe of 0-0048 failed with error -121
[   66.939620] cpu cpu0: "syscon" is missing, cannot use OPPv2 table.
[   66.946260] sdhci: Secure Digital Host Controller Interface driver
[   66.952465] sdhci: Copyright(c) Pierre Ossman
[   66.957586] omap_hsmmc 4809c000.mmc: [CCTV]omap_hsmmc_probe,eea7bc00
[   66.964059] [CCTV] mmc_alloc_host call dev_set_name ,mmc0
[   66.969490] [CCTV] mmc_of_parse call device_property_read_u32 ,mmc0
[   66.975908] omap_hsmmc 4809c000.mmc: Got CD GPIO
[   66.981333] omap_hsmmc 480b4000.mmc: [CCTV]omap_hsmmc_probe,eea7be00
[   66.987793] [CCTV] mmc_alloc_host call dev_set_name ,mmc0
[   66.993222] [CCTV] mmc_of_parse call device_property_read_u32 ,mmc0
[   67.000327] omap_hsmmc 480ad000.mmc: [CCTV]omap_hsmmc_probe,eea7c000
[   67.006807] [CCTV] mmc_alloc_host call dev_set_name ,mmc0
[   67.012237] [CCTV] mmc_of_parse call device_property_read_u32 ,mmc0
[   67.073759] sdhci-pltfm: SDHCI platform and OF driver helper,sdhci_pltfm_drv_init,259
[   67.086650] ledtrig-cpu: registered to indicate activity on CPUs
[   67.100357] omap_hwmod: mcasp3: _wait_target_ready failed: -16
[   67.106271] davinci-mcasp 48468000.mcasp: use pm_runtime_put_sync_suspend() in driver?
[   67.114271] ------------[ cut here ]------------
[   67.118921] WARNING: CPU: 0 PID: 1 at /home/cctv/tisdk/build/arago-tmp-external-linaro-toolchain/work-shared/am57xx-evm/kernel-source/drivers/bus/omap_l3_noc.c:147 l3_interrupt_handler+0x254/0x370
[   67.136468] 44000000.ocp:L3 Custom Error: MASTER MPU TARGET L4_PER2_P3 (Read): Data Access in User mode during Functional access
[   67.148080] Modules linked in:
[   67.151155] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.14.32-gdc3e450ded #5
[   67.158234] Hardware name: Generic DRA74X (Flattened Device Tree)
[   67.164354] Backtrace:
[   67.166821] [<c020b5fc>] (dump_backtrace) from [<c020b8e0>] (show_stack+0x18/0x1c)
[   67.174426]  r7:00000009 r6:60000193 r5:00000000 r4:c105366c
[   67.180115] [<c020b8c8>] (show_stack) from [<c091c8e8>] (dump_stack+0x90/0xa4)
[   67.187376] [<c091c858>] (dump_stack) from [<c022b6d8>] (__warn+0xec/0x104)
[   67.194369]  r7:00000009 r6:c0bccb64 r5:00000000 r4:ee87fae8
[   67.200059] [<c022b5ec>] (__warn) from [<c022b730>] (warn_slowpath_fmt+0x40/0x48)
[   67.207576]  r9:0000001a r8:eea0c290 r7:c0bcc9d0 r6:00000002 r5:c0bcca90 r4:c0bccb34
[   67.215358] [<c022b6f4>] (warn_slowpath_fmt) from [<c0519bcc>] (l3_interrupt_handler+0x254/0x370)
[   67.224266]  r3:eea0c100 r2:c0bccb34
[   67.227856]  r4:80080003
[   67.230408] [<c0519978>] (l3_interrupt_handler) from [<c027efe8>] (__handle_irq_event_percpu+0x6c/0x134)
[   67.239929]  r10:c105508d r9:eea09500 r8:00000017 r7:ee87fc0c r6:00000000 r5:eea09500
[   67.247790]  r4:eea0c600
[   67.250338] [<c027ef7c>] (__handle_irq_event_percpu) from [<c027f0d4>] (handle_irq_event_percpu+0x24/0x60)
[   67.260034]  r10:00000000 r9:ee87e000 r8:ee808000 r7:00000000 r6:c100936c r5:eea09500
[   67.267897]  r4:eea09500
[   67.270444] [<c027f0b0>] (handle_irq_event_percpu) from [<c027f150>] (handle_irq_event+0x40/0x64)
[   67.279353]  r5:eea09564 r4:eea09500
[   67.282949] [<c027f110>] (handle_irq_event) from [<c0282a24>] (handle_fasteoi_irq+0xac/0x160)
[   67.291512]  r7:00000000 r6:c100936c r5:eea09564 r4:eea09500
[   67.297200] [<c0282978>] (handle_fasteoi_irq) from [<c027e238>] (generic_handle_irq+0x2c/0x3c)
[   67.305848]  r7:00000000 r6:00000000 r5:00000017 r4:c0e63afc
[   67.311532] [<c027e20c>] (generic_handle_irq) from [<c027e7c0>] (__handle_domain_irq+0x64/0xbc)
[   67.320271] [<c027e75c>] (__handle_domain_irq) from [<c0201474>] (gic_handle_irq+0x44/0x80)
[   67.328661]  r9:ee87e000 r8:fa213000 r7:fa212000 r6:ee87fcc8 r5:fa21200c r4:c1004000
[   67.336440] [<c0201430>] (gic_handle_irq) from [<c020c4b8>] (__irq_svc+0x58/0x8c)
[   67.343954] Exception stack(0xee87fcc8 to 0xee87fd10)
[   67.349028] fcc0:                   eea7e210 00000005 00000000 eea7e2e4 eea7e210 00000005
[   67.357243] fce0: 00000000 edc5a590 00000000 00000000 00000000 ee87fd34 ee87fd38 ee87fd18
[   67.365455] fd00: c07dfb88 c0655634 20000013 ffffffff
[   67.370529]  r9:ee87e000 r8:00000000 r7:ee87fcfc r6:ffffffff r5:20000013 r4:c0655634
[   67.378318] [<c0655610>] (__pm_runtime_idle) from [<c07dfb88>] (davinci_mcasp_probe+0xa38/0xb88)
[   67.387141]  r7:edc5a590 r6:00000000 r5:eea7e210 r4:edc4fa10
[   67.392830] [<c07df150>] (davinci_mcasp_probe) from [<c064d058>] (platform_drv_probe+0x58/0xb4)
[   67.401568]  r10:00000000 r9:00000000 r8:c104c2e4 r7:fffffdfb r6:c104c2e4 r5:ffffffed
[   67.409428]  r4:eea7e210
[   67.411977] [<c064d000>] (platform_drv_probe) from [<c064b594>] (driver_probe_device+0x240/0x2f0)
[   67.420886]  r7:00000000 r6:c10953fc r5:c10953f8 r4:eea7e210
[   67.426572] [<c064b354>] (driver_probe_device) from [<c064b6f0>] (__driver_attach+0xac/0xb0)
[   67.435046]  r10:c1058000 r9:000000d1 r8:c0e49834 r7:00000000 r6:eea7e244 r5:c104c2e4
[   67.442907]  r4:eea7e210 r3:00000000
[   67.446501] [<c064b644>] (__driver_attach) from [<c06498cc>] (bus_for_each_dev+0x54/0xa4)
[   67.454711]  r7:00000000 r6:c064b644 r5:c104c2e4 r4:00000000
[   67.460398] [<c0649878>] (bus_for_each_dev) from [<c064af10>] (driver_attach+0x24/0x28)
[   67.468436]  r6:c1032650 r5:edc5a500 r4:c104c2e4
[   67.473075] [<c064aeec>] (driver_attach) from [<c064aa24>] (bus_add_driver+0x190/0x214)
[   67.481117] [<c064a894>] (bus_add_driver) from [<c064c060>] (driver_register+0x80/0xfc)
[   67.489155]  r7:c1058000 r6:c0e3460c r5:00000000 r4:c104c2e4
[   67.494841] [<c064bfe0>] (driver_register) from [<c064cfb0>] (__platform_driver_register+0x48/0x50)
[   67.503923]  r5:00000000 r4:c1032650
[   67.507519] [<c064cf68>] (__platform_driver_register) from [<c0e34628>] (davinci_mcasp_driver_init+0x1c/0x20)
[   67.517474]  r5:00000000 r4:ffffe000
[   67.521068] [<c0e3460c>] (davinci_mcasp_driver_init) from [<c02019fc>] (do_one_initcall+0x4c/0x170)
[   67.530159] [<c02019b0>] (do_one_initcall) from [<c0e00f80>] (kernel_init_freeable+0x1d8/0x274)
[   67.538894]  r8:c0e49834 r7:c1058000 r6:00000007 r5:c0e5c2b0 r4:c0c7eb34
[   67.545629] [<c0e00da8>] (kernel_init_freeable) from [<c092f980>] (kernel_init+0x10/0x110)
[   67.553928]  r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c092f970
[   67.561788]  r4:00000000
[   67.564338] [<c092f970>] (kernel_init) from [<c0207d98>] (ret_from_fork+0x14/0x3c)
[   67.571938]  r5:c092f970 r4:00000000
[   67.575535] ---[ end trace 315fdbf6e4e3c32d ]---
[   67.581423] Unhandled fault: asynchronous external abort (0x1211) at 0x00000000
[   67.588764] pgd = c0003000
[   67.591482] [00000000] *pgd=80000080004003, *pmd=00000000
[   67.596916] Internal error: : 1211 [#1] PREEMPT SMP ARM
[   67.602162] Modules linked in:
[   67.605235] CPU: 0 PID: 1 Comm: swapper/0 Tainted: G        W       4.14.32-gdc3e450ded #5
[   67.613535] Hardware name: Generic DRA74X (Flattened Device Tree)
[   67.619652] task: ee880000 task.stack: ee87e000
[   67.624206] PC is at __pm_runtime_idle+0x24/0x88
[   67.628844] LR is at davinci_mcasp_probe+0xa38/0xb88
[   67.633830] pc : [<c0655634>]    lr : [<c07dfb88>]    psr: 20000013
[   67.640123] sp : ee87fd18  ip : ee87fd38  fp : ee87fd34
[   67.645368] r10: 00000000  r9 : 00000000  r8 : 00000000
[   67.650614] r7 : edc5a590  r6 : 00000000  r5 : 00000005  r4 : eea7e210
[   67.657169] r3 : eea7e2e4  r2 : 00000000  r1 : 00000005  r0 : eea7e210
[   67.663726] Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
[   67.670892] Control: 30c5387d  Table: 80003000  DAC: fffffffd
[   67.676663] Process swapper/0 (pid: 1, stack limit = 0xee87e210)
[   67.682695] Stack: (0xee87fd18 to 0xee880000)
[   67.687069] fd00:                                                       edc4fa10 eea7e210
[   67.695283] fd20: 00000000 edc5a590 ee87fdcc ee87fd38 c07dfb88 c065561c 00002000 edc58890
[   67.703497] fd40: edc4fa10 c0bd89c0 00000001 00000000 ee87fd74 00000020 eed5648c 00000002
[   67.711709] fd60: 00000084 00000001 ee87fd94 00000000 edc5bc60 c0bdf6c4 edc5bd20 00000001
[   67.719924] fd80: eea792a0 00000000 ee87fdbc ee87fd98 c03a6764 c03a2ca4 eea7e210 00000000
[   67.728136] fda0: eea7e218 eea7e210 ffffffed c104c2e4 fffffdfb c104c2e4 00000000 00000000
[   67.736351] fdc0: ee87fdec ee87fdd0 c064d058 c07df15c eea7e210 c10953f8 c10953fc 00000000
[   67.744566] fde0: ee87fe1c ee87fdf0 c064b594 c064d00c 00000000 eea7e210 c104c2e4 eea7e244
[   67.752781] fe00: 00000000 c0e49834 000000d1 c1058000 ee87fe3c ee87fe20 c064b6f0 c064b360
[   67.760993] fe20: 00000000 c104c2e4 c064b644 00000000 ee87fe64 ee87fe40 c06498cc c064b650
[   67.769208] fe40: ee862858 eea6ed34 ee86286c c104c2e4 edc5a500 c1032650 ee87fe74 ee87fe68
[   67.777419] fe60: c064af10 c0649884 ee87fe9c ee87fe78 c064aa24 c064aef8 c0c25ff4 ee87fe88
[   67.785633] fe80: c104c2e4 00000000 c0e3460c c1058000 ee87feb4 ee87fea0 c064c060 c064a8a0
[   67.793845] fea0: c1032650 00000000 ee87fecc ee87feb8 c064cfb0 c064bfec ffffe000 00000000
[   67.802060] fec0: ee87fedc ee87fed0 c0e34628 c064cf74 ee87ff4c ee87fee0 c02019fc c0e34618
[   67.810272] fee0: ee87ff4c ee87fef0 c0247e00 c0e00624 c0ba17dc c0ba17bc c0ba1808 c0baed98
[   67.818485] ff00: 00000000 c0ba1794 00000006 00000006 c0c002a8 c0c7eb34 effff804 00000000
[   67.826698] ff20: 00000000 c0c7eb34 00000007 c0c7eb34 c0e5c2b0 00000007 c1058000 c0e49834
[   67.834914] ff40: ee87ff94 ee87ff50 c0e00f80 c02019bc 00000006 00000006 00000000 c0e00618
[   67.843127] ff60: 0040a188 c0e00618 444a220c 00000000 c092f970 00000000 00000000 00000000
[   67.851340] ff80: 00000000 00000000 ee87ffac ee87ff98 c092f980 c0e00db4 00000000 c092f970
[   67.859553] ffa0: 00000000 ee87ffb0 c0207d98 c092f97c 00000000 00000000 00000000 00000000
[   67.867767] ffc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[   67.875978] ffe0: 00000000 00000000 00000000 00000000 00000013 00000000 0854d432 0460c006
[   67.884188] Backtrace:
[   67.886654] [<c0655610>] (__pm_runtime_idle) from [<c07dfb88>] (davinci_mcasp_probe+0xa38/0xb88)
[   67.895478]  r7:edc5a590 r6:00000000 r5:eea7e210 r4:edc4fa10
[   67.901167] [<c07df150>] (davinci_mcasp_probe) from [<c064d058>] (platform_drv_probe+0x58/0xb4)
[   67.909906]  r10:00000000 r9:00000000 r8:c104c2e4 r7:fffffdfb r6:c104c2e4 r5:ffffffed
[   67.917768]  r4:eea7e210
[   67.920314] [<c064d000>] (platform_drv_probe) from [<c064b594>] (driver_probe_device+0x240/0x2f0)
[   67.929226]  r7:00000000 r6:c10953fc r5:c10953f8 r4:eea7e210
[   67.934913] [<c064b354>] (driver_probe_device) from [<c064b6f0>] (__driver_attach+0xac/0xb0)
[   67.943388]  r10:c1058000 r9:000000d1 r8:c0e49834 r7:00000000 r6:eea7e244 r5:c104c2e4
[   67.951252]  r4:eea7e210 r3:00000000
[   67.954844] [<c064b644>] (__driver_attach) from [<c06498cc>] (bus_for_each_dev+0x54/0xa4)
[   67.963056]  r7:00000000 r6:c064b644 r5:c104c2e4 r4:00000000
[   67.968744] [<c0649878>] (bus_for_each_dev) from [<c064af10>] (driver_attach+0x24/0x28)
[   67.976780]  r6:c1032650 r5:edc5a500 r4:c104c2e4
[   67.981419] [<c064aeec>] (driver_attach) from [<c064aa24>] (bus_add_driver+0x190/0x214)
[   67.989459] [<c064a894>] (bus_add_driver) from [<c064c060>] (driver_register+0x80/0xfc)
[   67.997499]  r7:c1058000 r6:c0e3460c r5:00000000 r4:c104c2e4
[   68.003188] [<c064bfe0>] (driver_register) from [<c064cfb0>] (__platform_driver_register+0x48/0x50)
[   68.012270]  r5:00000000 r4:c1032650
[   68.015866] [<c064cf68>] (__platform_driver_register) from [<c0e34628>] (davinci_mcasp_driver_init+0x1c/0x20)
[   68.025823]  r5:00000000 r4:ffffe000
[   68.029416] [<c0e3460c>] (davinci_mcasp_driver_init) from [<c02019fc>] (do_one_initcall+0x4c/0x170)
[   68.038505] [<c02019b0>] (do_one_initcall) from [<c0e00f80>] (kernel_init_freeable+0x1d8/0x274)
[   68.047243]  r8:c0e49834 r7:c1058000 r6:00000007 r5:c0e5c2b0 r4:c0c7eb34
[   68.053976] [<c0e00da8>] (kernel_init_freeable) from [<c092f980>] (kernel_init+0x10/0x110)
[   68.062278]  r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c092f970
[   68.070140]  r4:00000000
[   68.072689] [<c092f970>] (kernel_init) from [<c0207d98>] (ret_from_fork+0x14/0x3c)
[   68.080288]  r5:c092f970 r4:00000000
[   68.083882] Code: e1a04000 0a00000a f57ff05b e28030d4 (f593f000)
[   68.090012] ---[ end trace 315fdbf6e4e3c32e ]---
[   68.095872] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[   68.095872]
[   68.105056] CPU1: stopping
[   68.107779] CPU: 1 PID: 0 Comm: swapper/1 Tainted: G      D W       4.14.32-gdc3e450ded #5
[   68.116080] Hardware name: Generic DRA74X (Flattened Device Tree)
[   68.122197] Backtrace:
[   68.124663] [<c020b5fc>] (dump_backtrace) from [<c020b8e0>] (show_stack+0x18/0x1c)
[   68.132267]  r7:fa212000 r6:20000193 r5:00000000 r4:c105366c
[   68.137953] [<c020b8c8>] (show_stack) from [<c091c8e8>] (dump_stack+0x90/0xa4)
[   68.145212] [<c091c858>] (dump_stack) from [<c020ebb8>] (handle_IPI+0x1b8/0x1cc)
[   68.152642]  r7:fa212000 r6:00000001 r5:00000000 r4:c0e63afc
[   68.158329] [<c020ea00>] (handle_IPI) from [<c02014ac>] (gic_handle_irq+0x7c/0x80)
[   68.165933]  r6:ee8a3f20 r5:fa21200c r4:c1004000
[   68.170572] [<c0201430>] (gic_handle_irq) from [<c020c4b8>] (__irq_svc+0x58/0x8c)
[   68.178084] Exception stack(0xee8a3f20 to 0xee8a3f68)
[   68.183158] 3f20: 00000001 00000000 00000000 c02197e0 ffffe000 c1003cd8 c1003c78 00000000
[   68.191371] 3f40: 00000000 c0e633b8 c1003ce4 ee8a3f7c ee8a3f80 ee8a3f70 c0208858 c020885c
[   68.199582] 3f60: 60000013 ffffffff
[   68.203086]  r9:ee8a2000 r8:00000000 r7:ee8a3f54 r6:ffffffff r5:60000013 r4:c020885c
[   68.210873] [<c020881c>] (arch_cpu_idle) from [<c09350fc>] (default_idle_call+0x28/0x34)
[   68.219003] [<c09350d4>] (default_idle_call) from [<c026b090>] (do_idle+0x194/0x224)
[   68.226780] [<c026aefc>] (do_idle) from [<c026b3e4>] (cpu_startup_entry+0x20/0x24)
[   68.234384]  r10:00000000 r9:412fc0f2 r8:80007000 r7:c1058250 r6:00000001 r5:ee8a2000
[   68.242246]  r4:00000084
[   68.244794] [<c026b3c4>] (cpu_startup_entry) from [<c020e77c>] (secondary_start_kernel+0x170/0x17c)
[   68.253883] [<c020e60c>] (secondary_start_kernel) from [<802017ac>] (0x802017ac)
[   68.261313]  r7:c1058250 r6:30c0387d r5:00000000 r4:ae84aac0
[   68.267006] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[   68.267006]