Part Number: AM5718
Other Parts Discussed in Thread: DM3730,
Tool/software: Linux
HI everybody ,
I am using a configuration used in the past on DM3730 and working there .
Now in my boards is presents a USB hub, with 2 USB ports, connected to an AM5718 processor; we need to test the USB overcurrent functionality in two different cases:
A - when a generic load is plugged in the USB connector, e.g. a LED lamp
B - when a standard USB device is used
We have these results with Kernel 4.9 rt:
- case A: overcurrent event is not generated
- case B: overcurrent event is correctly generated
- case A in one port and B in the second port: overcurrent event is correctly generated
This behaviour is different from the one we have in one of our boards with the same hardware but for the DM3730 processor with Kernel 2.6.32 where USB OVERCURRENT always occurs.
thank you very much
regards
Carlo