Part Number: TDA2
Hi,
These are the steps I'm following to run the dsp_test_dl_algo.out.
1.Open CCS. Launch Selected Configuration.
2.Select A15_0. Go to Run->Reset->System Reset. Right click-> Connect Target. Go to Scripts->TDA2xx MULTICORE Initialization->TDA2xx_MULTICORE_EnableAllCores
3.Select C6xx_DSP1. Right click->Connect Target.
4.Go to Run->Load->Load Program. Select the path of dsp_test_dl_algo.out. file and click Ok.
5.Click on Resume button.
In the console I am seeing these logs.
[C66xx_DSP1]
Processing config file ..\testvecs\config\infer\tidl_config_jseg21.txt !
and nothing after that. Do any more configuration need to be done or is there anything wrong with the configuration I am currently setting?
Thanks in advance,
Navinprashath.R.R