This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748 USB2.0 CDMA Double Packet Buffering

Expert 4270 points

Hi Champ !

My customer asked regarding to C6748 USB CDMA usage.

Assumption is they are using "Peripheral Mode".

They try to use CDMA (Transparent mode) and will be enabled "Double Packet Buffering" (DPB=1 of TXFIFOSZ and RXFIFOSZ)

then transmit and receive will be failure.

1, Is it impossible to use CDMA(Transparent mode) and Double Packet Buffering simultaneously ?

2, How about a RNDIS mode ?

When they try to receive a data by using CDMA, if the data which is exceeded length than the "Host Packet Descriptor" registered will come,

there is NO receive interrupt occurred. (also there is NO error interrupt occurred)

3, Is there any solution to detect when the big data which is exceeded buffer length size will come ?

Your quick response would be great appreciate !

Thanks in advance.

Best Regards.

PIC Japan Obara.