This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: LCD driver in U-boot

Part Number: PROCESSOR-SDK-AM335X

Tool/software: Linux

hi.. i need your help :)

i try to adding splash screen in my u-boot 2017.09,i use paralel LCD G057vn01, i have done follow tutorial from

when i install it in my device and debug it from console, see like this:

U-Boot 2017.09 (May 08 2018 - 18:12:51 +0700)                                   
                                                                                
CPU  : AM335X-GP rev 2.1                                                        
I2C:   ready                                                                    
DRAM:  512 MiB                                                                  
No match for driver 'omap_hsmmc'                                                
No match for driver 'omap_hsmmc'                                                
Some drivers were not found                                                     
Reset Source: Power-on reset has occurred.                                      
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1                                           
Using default environment                                                       
                                                                                
Board: BeagleBone Black                                                         
~~~~~~ SPLASH SCREEN ~~~~~~                                                     
~~~~~~~ MMC FOUNDED ~~~~~~~                                                     
reading splash.bmp.gz                                                           
<ethaddr> not set. Validating first E-fuse MAC                                  
Net:   eth0: MII MODE                                                           
cpsw                                                                            
Press SPACE to abort autoboot in 2 seconds                                      
board_name=[A335BNLT] ...                                                       
board_rev=[000C] ...                                                            
switch to partitions #0, OK                                                     
mmc0 is current device                                                          
SD/MMC found on device 0                                                        
** Bad device 0:2 0x82000000 **                                                 
** Bad device 0:2 0x82000000 **                                                 
switch to partitions #0, OK                                                     
mmc0 is current device                                                          
Scanning mmc 0:1...                                                             
gpio: pin 56 (gpio 56) value is 0                                               
gpio: pin 55 (gpio 55) value is 0                                               
gpio: pin 54 (gpio 54) value is 0                                               
gpio: pin 53 (gpio 53) value is 1                                               
switch to partitions #0, OK                                                     
mmc0 is current device                                                          
gpio: pin 54 (gpio 54) value is 1                                               
Checking for: /uEnv.txt ...                                                     
reading uEnv.txt                                                                
1179 bytes read in 4 ms (287.1 KiB/s)                                           
gpio: pin 55 (gpio 55) value is 1                                               
Loaded environment from /uEnv.txt                                               
Importing environment from mmc ...                                              
Checking if uenvcmd is set ...                                                  
gpio: pin 56 (gpio 56) value is 1                                               
Running uenvcmd ...                                                             
1757 bytes read in 30 ms (56.6 KiB/s)                                           
debug: [/boot/vmlinuz-3.8.13-bone79] ...

it can reading my "splash.bmp.gz" but i don't see anything in my LCD, whats wrong?