This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Max CLK for mDDR

One of the posts here mentioned the max CLK supported by DM355 is 133MHz. Is that the max frequency. It seems kind of strange that max frequency supported just happened to match one of the rated frequencies for mDDR chips. Especially when (from what I understand) it is not possible to set the maximum frequency to 133MHz exactly. What timing parameters limit the maximum frequency? Is there more information describing the limit?

Thank you.