This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AM5728: RTOS USB Host MSC example error

Part Number: AM5728


Tool/software: TI-RTOS

Hi,

I'm experiencing an issue with running the USB mass-storage host example application on evmAM5728 board.

PDK version: pdk_am57xx_1_0_10

CCS version: 8.0.0.00016 

cd C:\ti\pdk_am57xx_1_0_10\packages

pdksetupenv.bat

pdkProjectCreate.bat AM572x idkAM572x little usb all arm

Build the imported project, connect to ARM core then load the .out file and run the program. The CCS ConsoleIO will display the following:

RTOS USB Host MSC example!!
USBHCDMain failed with this error: 0xf0000

 

Best regards,

Omid