HI:
I want to use mem copy with dma ,use function Utils_dmaCopy1D,but I find the dest memory is not work ok. the data is always 0. ( dma callback can be work,but the data is not right);
how can i let it work right with Utils_DmaCopy1D.
THANK YOU!
the code as follow below:
void dma_memtest()
{
Utils_DmaChCreateParams dmaChPrm;
Utils_DmaChObj dmaobj;
Utils_DmaCopy1D dmaParams;
Int32 status;
dmaChPrm.eventQ = 0;
Utils_DmaChCreateParams_Init(&dmaChPrm);
status = Utils_dmaCreateCh(
&dmaobj,
&dmaChPrm
);
UTILS_assert(status == SYSTEM_LINK_STATUS_SOK);
gspidestBUf = Utils_memAlloc
(
UTILS_HEAPID_DDR_CACHED_SR,
1024,
4
);
gspisrcBUf = Utils_memAlloc
(
UTILS_HEAPID_DDR_CACHED_SR,
1024,
4
);
memset(gspisrcBUf,0x77,300);
dmaParams.destAddr = gspidestBUf;
dmaParamsrcAddr =(Ptr)gspisrcBUf;//(Ptr)0x4809a13C;
dmaParams.length =32;
Utils_dmaCopy1D(&dmaobj, &dmaParams);
Utils_dmaDeleteCh(&dmaobj);
HexToStr(tmp,gspisrcBUf,32);
Vps_printf("\r\nsrc:");
Vps_printf((const char*)tmp);
Vps_printf("\r\n");
HexToStr(tmp,gspidestBUf,32);
Vps_printf("\r\ndst:");
Vps_printf((const char*)tmp);
Vps_printf("\r\n");
}