Tool/software: Linux
Hello Team,
We are using custom h/w and software based on DRA746 and SDK 3.03.
We are trying to play subtitle and videos on two different surfaces, because currently we are using SW composition for subtitles and this is causing memory issues in the system.
So we are trying to have subtitles on different surface and video on other suraface and let wayland take cares the composition in HW. Currently we are working on this.Please correct me if we are missing anything or if this approach looks ok.
One more thing, is it possible to play a subtitle file without video file, if yes please share the pipeline for the same.
we are using this pipeline but not working:
gst-launch-1.0 filesrc location=/tmp/USB1-1.4-sda1/2-H264\(640360_30\)MP3\(128_44\).srt ! ia_subparse ! textrender ! videoconvert ! 'video/x-raw,format=(string)AYUV' ! waylandsink
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
ERROR: from element /GstPipeline:pipeline0/GstTextRender:textrender0: GStreamer error: negotiation problem.
Additional debug info:
/home/buildserver/work/jenkins/var/lib/jenkins/workspace/MMT2020-ADV-R3-0-Customer-Release-Builds/project/elina-distro/build-cpm-mmt-2020/tmp/work/cortexa15hf-vfp-neon-elina-linux-gnueabi/gstreamer1.0-plugins-base/1.6.3-r0/gst-plugins-base-1.6.3/ext/pango/gsttextrender.c(511): gst_text_render_chain (): /GstPipeline:pipeline0/GstTextRender:textrender0
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Freeing pipeline ...
Thanks & Regards,
Ikshwaku