In the DDR2/DDR3 interface design, can we swap DQs with in the same byte? is there any rules on this?
such as dq0 swapped with dq3
dq2 with dq7, etc
Thanks
Jianming
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the DDR2/DDR3 interface design, can we swap DQs with in the same byte? is there any rules on this?
such as dq0 swapped with dq3
dq2 with dq7, etc
Thanks
Jianming
Hi,
Yes, it is okay to swap DQ bits within the same byte on the TDA2x DDR2/DDR3 interface. The only rule for DQ bit swapping on the TDA2x DDR2/DDR3 interface is that the DQ bits must be routed with their associated strobe (DQS) and mask (DM). (i.e, all signals within a byte of the TDA2x must be routed to the same byte of the DDR2/3 memory).
Best regards,
Kevin