This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVMOMAPL137 - EMAC loopback



I try to test the EMAC with the BSL EMAC looback test (BSL->dsp->tests->emac_loopback)

The test seems to work incorrectly.

There are some errors in the validation of incoming packets.

I think there is some bug during a configuration of the PHY chip.

I use CCSv4.2+XDS510 USB emulator

Maybe I use the test incorrectly?

I expect the test should work with the PHY chip internal loopback.

Maybe it should work with some host test application?

The EVM is OK because the NDK client test application works fine.

Best regards,

Yuriy