This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM4376: EMIF PHY settings

Part Number: AM4376

Tool/software: Linux

Hi Sir 

We are using AM4376 with latest sdk for development. 

we have some questions about ext_phy_settings_hwlvl function in ddr.c of u-boot.

static void ext_phy_settings_hwlvl(const struct emif_regs *regs, int nr)
{
/*
* Enable hardware leveling on the EMIF. For details about these
* magic values please see the EMIF registers section of the TRM.
*/
writel(0x08020080, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_1);
writel(0x08020080, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_1_shdw);
writel(0x00000000, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_22);
writel(0x00000000, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_22_shdw);
writel(0x00600020, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_23);
writel(0x00600020, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_23_shdw);
writel(0x40010080, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_24);
writel(0x40010080, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_24_shdw);
writel(0x08102040, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_25);
writel(0x08102040, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_25_shdw);
writel(0x00200020, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_26);
writel(0x00200020, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_26_shdw);
writel(0x00200020, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_27);
writel(0x00200020, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_27_shdw);
writel(0x00200020, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_28);
writel(0x00200020, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_28_shdw);
writel(0x00200020, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_29);
writel(0x00200020, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_29_shdw);
writel(0x00200020, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_30);
writel(0x00200020, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_30_shdw);
writel(0x00000000, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_31);
writel(0x00000000, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_31_shdw);
writel(0x00000000, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_32);
writel(0x00000000, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_32_shdw);
writel(0x00000000, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_33);
writel(0x00000000, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_33_shdw);
writel(0x00000000, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_34);
writel(0x00000000, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_34_shdw);
writel(0x00000000, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_35);
writel(0x00000000, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_35_shdw);
writel(0x000000FF, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_36);
writel(0x000000FF, &emif_reg[nr]->emif_ddr_ext_phy_ctrl_36_shdw);

/*
* Sequence to ensure that the PHY is again in a known state after
* hardware leveling.
*/
writel(0x2011, &emif_reg[nr]->emif_iodft_tlgc);
writel(0x2411, &emif_reg[nr]->emif_iodft_tlgc);
writel(0x2011, &emif_reg[nr]->emif_iodft_tlgc);
}

we didn't find the source code to write the register from emif_ddr_ext_phy_ctrl_2 ~ emif_ddr_ext_phy_ctrl_21.

Is there something wrong or it is not necessary to write register from emif_ddr_ext_phy_ctrl_2 ~ emif_ddr_ext_phy_ctrl_21 in ext_phy_settings_hwlvl api.

please advise

BR

Yimin