This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM4376: Issue with WoW interrupt pin

Part Number: AM4376

Tool/software: Linux

Hi everyone,

I'm having an issue on a custom board using AM4376, linux 4.4.19, with WoW not working. We want to change the interrupt pin, which is gpio0[19] in TI documentation (cf patch in following link), to gpio0[14].

The problem come from the interrupt pin not working as expected. For easy debugging we've put a button on gpio0[14] (K21). Value is set to 1 by default, and set to 0 when pushed.

We put our board in suspend to ram using "echo mem > /sys/power/state", and try to wake up using out button, but this is not working (nothing happen). For information, we can successfully wake up using uart0.

I've modified DTS following this documentation , and more precisely this patch.

I've made the same test on several available GPIO (gpio4[8] and gpio 4[11]), with the same result.

The main question is: can we use another GPIO than gpio0[19] as mentioned in the patch ? Do we need to configure something else than DTB ?

Thanks for your help.

Best regards,

J.L.