Hello,
I have been going through the manuals, but I can't find an authoritative answer. I am feeding a 720p Video Source signal into the DM648's Video Port and I have it set it up for Progressive Scan mode (Capture Field 1 only). When I am in that mode, are the Field 2 registers (VCXSTART2, VCXSTOP2, VCYSTART2, VCYSTOP2) completely ignored so that a value of 0x0 in those registers doesn't affect anything, or must I put in valid values even though I don't capture Field 2?
There is no possibility that the Video Port is capturing the next Progressive Frame in a Field 2 slot, is there?
What is a full recommended setup for 720p for Video Port capture registers?
Sorry to ask all these questions, but the Data manuals do not explain this very well.....Like everything else, they only explain in detail everything setup for the Field 1 only capture scenario and totally ignore any mention of the Field 2 implications of the device in this mode. It would be very nice if the manual stated that the Field 2 registers are totally ignored in the Field 1 only Capture mode, if that is truly the case.
Thanks,