Hi
i run the encode demo on dm365(DVSDK2.1) as follow to get a g711 file using the mic on the EVM board: ./encode -t 10 -v test.264 -s test.g711, but it shows failed to create speech device. I use the kernel with default configuration, someone says the kernel must contain the cq93VC modules, so i build a new kernel, but the problem always existed.
so who can tell me the reason?
thx