Part Number: TDA3LX
Hi expert,
Customer want to run TFDTP on their own board with Radar SDK 3.03. Currently TCP/IP connection test is passed. Then we add TFDTP TX link based on framecopy demo but the connection failed. As below is the log from customer, could you please help to give some suggestion? Thank you.
IPU1-0 Remote Log Shared Memory @ 0xbfee00a0
[Cortex_M4_IPU1_C1]
[Cortex_M4_IPU1_C0] IPU1-1 Remote Log Shared Memory @ 0xbfeee8a0
[Cortex_M4_IPU1_C1] MAC Port 0 Address:
[Cortex_M4_IPU1_C0] HOST Remote Log Shared Memory @ 0xbfef10a0
[Cortex_M4_IPU1_C1] 58-7a-62-95-03-88
[Cortex_M4_IPU1_C0] DSP1 Remote Log Shared Memory @ 0xbfef60a0
[Cortex_M4_IPU1_C1]
[Cortex_M4_IPU1_C0] DSP2 Remote Log Shared Memory @ 0xbfef88a0
[Cortex_M4_IPU1_C1] MAC Port 1 Address:
[Cortex_M4_IPU1_C0] EVE1 Remote Log Shared Memory @ 0xbfefb0a0
[Cortex_M4_IPU1_C1] 58-7a-62-95-03-89
[Cortex_M4_IPU1_C0] EVE2 Remote Log Shared Memory @ 0xbfefd8a0
EVE3 Remote Log Shared Memory @ 0xbff000a0
EVE4 Remote Log Shared Memory @ 0xbff028a0
IPU2 Remote Log Shared Memory @ 0xbff050a0
[Cortex_M4_IPU1_C1] GMACSW has been started successfully
Registration of the GMACSW Successful
Service Status: DHCPC : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
[Cortex_M4_IPU1_C0]
i2cMdSubmitChan: i2c0 transfer to slave address 0x51 failed
i2cMdSubmitChan: i2c0 transfer to slave address 0x51 failed
i2cMdSubmitChan: i2c0 transfer to slave address 0x20 failed
i2cMdSubmitChan: i2c0 transfer to slave address 0x20 failed
i2cMdSubmitChan: i2c0 transfer to slave address 0x23 failed
SYSTEM: UART: INTERRUPT Mode is Selected
[Cortex_M4_IPU1_C1] Negotiated connection: FullDuplex 1000 Mbs
[Cortex_M4_IPU1_C0]
i2cMdSubmitChan: i2c0 transfer to slave address 0x20 failed
i2cMdSubmitChan: i2c0 transfer to slave address 0x20 failed
i2cMdSubmitChan: i2c0 transfer to slave address 0x23 failed
SYSTEM: UART: INTERRUPT Mode is Selected
After a while,
[Cortex_M4_IPU1_C1] Service Status: DHCPC : Enabled : Fault : 002
Regards,
Allen