This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SVGA (800x600 @ 60Hz) source for TVP7002

Other Parts Discussed in Thread: TVP7002

Hello all,

I am trying to use DM6467 with TVP7002 to capture 800x600@60Hz graphics input. I tried using VGA to RGB cable as analog RGB source for my experiment. The cable has 15 pin VGA connector on one end and 3 RGB-RCA jack on the other hand. I am connecting the VGA end of the cable to CPU and 3 RCA jacks to TVP7002 component input. Below are my questions:

1) Can I use such setup as source for this experiment?

2) Is there any other option except video pattern generator for graphics inputs in my experiment?

When I tried to use such analog source, TVP7002 detects random number of lines. I am reading number of lines using reg 37h and 38h.

Thank you for any suggestion.

- Bhavin