Hello,
We are trying to connect to LAN with PC using custom board with Vision-SDK 3.02 and TDA 3 (different configuration from EVM).
TDA 3 recognizes that there are two pins for ETHERNET, RGMii 0 and RGMII 1.
Where should I change to switch between RGMII 0 and RGMII 1?
Also, although the AR8031 installed on the EVM board seems to be compatible with 1000 BASE - X and 100 BASE - FX, where can I switch this function?
* We are planning to give RGM II 0 and RGM II 1 different functions in the future respectively.
Thanks and regard.