This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EVM5777: TDA2EVM5777

Part Number: TDA2EVM5777
Other Parts Discussed in Thread: TDA2

Hello 

I'm building a ADAS with TDA2

the OV10640 is in the TDA2 AVL

but I want to use OV10642

the only difference between them is the optical filter

so can I use OV10642 in TDA2?

if yes

is now TDA2 support parallel interface to OV10642? or when could TDA2 support parallel interface to OV10642?

thank you