Other Parts Discussed in Thread: OMAP3530
We have a requirement for developing a Image processing Platform where our basic set up
contains Two CCD camera at the front end and support for VGA AND LCD module to display the Live view simultaneously with real time graphics overlay.
The central processor will perform some image processing like edge detection, threshold, feature extraction on both the images in real time at the rate of 10 images per sec
Here we some components like LCD module, CCTV CCD camera(PAL).
We want complete development set up based on texas instruments media processors and
the initial cost of the IDE, development boards etc, and sutable processor like OMAP or X6446
or DaVinci etc.
Can anybody please help us to find the suitable solution for this type of application