Part Number: TDA3-Q1
Hello,
We've developed our system with AWR1243 and TDA3. We're migrating Radar SDK from v2.12 to v3.02.
In Radar SDK v2.12, we got advice from TI to set SYSTEM_CSI2_RAW8 to inCsi2DataFormat.
<RadarSDKv2.12>\vision_sdk\examples\tda2xx\src\radar\src\common\chains_common_ar12xx.c
In Radar SDK v3.02, I think SYSTEM_CSI2_RAW8 should be set like v2.12.
<RadarSDKv3.02>\vision_sdk\apps\src\rtos\radar\src\common\chains_common_ar12xx.c
In v3.02, SYSTEM_CSI2_RAWx seems to be determined depending on the ADC data format (12, 14 and 16-bit). (By the way, the A2D resolution of AWR1243 is 12-bit, I'm not sure that meaning.)
Should I set "#define CHAINS_AR1243_ADC_DATA_FORMAT (16U)" as default and select "#define CHAINS_AR1243_CSI_CAPTURE_DATA_FORMAT (SYSTEM_CSI2_RAW8) / * 16 bit * /" ?
Please give me some advice.
Regards,
Kazu