Tool/software: Linux
Hi,
We have a custom board based on AM437x IDK.
We are currently booting from QSPI flash. Uboot version from the SDK is 2017.1
The issue is, if we dont connect the serial debug cable to the board and to the host PC, Uboot is stuck at auto boot prompt.
I tired disabling the boot delay(bootDelay=0) to ensure any noise from the UART is not feeding distorted characters to auto boot command prompt.
Still Uboot is stuck Autoboot prompt before starting the kernel.
If I connect the serial cable at this point, type the boot command, Uboot boots the kernel successfully.
The defconfig used for QSPI boot mode: am43xx_evm_qspiboot_defconfig
Please let me know if you have any inputs for this issue.
Thannks in advance
Rohit