This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Easiest way to configure DM6437's cache, timer, etc, without using DSP/BIOS?

Hi,

In order to test the performance of my algorithm, I need to configure cache, timer, etc on DM6437. I also need file I/O for test vector purpose, so I can't use DSP/BIOS yet.

This used to be very simple with the CSL API; now that a CSL is no longer available for DM6437, I'll have to hand code the registers. It's not difficult, but quite tedious and error prone.

Is there a better way? And, out of curiosity, why doesn't TI simply provide a CSL for DM6437?

Thanks,