This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to burn uboot into Flash?



Hi , I'm using EVM6446.   I know I can use JTAG to finish this work.  But I don't want to use JTAG to burn uboot into Flash, I want to burn uboot via "ttyS0" (serial port).

I mean:

I want to write an application in PC host (Linux), in this application I want to "open" ttyS0 and pass uboot.bin into Flash on EVM.  

1) In this application I think I can open "ttyS0", but I do not  know an exact memory address of Flash on EVM board,  so I don't know where I should write "uboot.bin" to.

2) Even if I know the address of Flash on EVM board, how can I tell EVM " now I want to write something in the memeory address?

Could anyone tell me what I should do or some references?

Thanks.

 

Lorry