Part Number: AM5728
Other Parts Discussed in Thread: TLK105,
Hi everybody ,
I am on IDK kit and have some questions on Ethercat LED activation :
1--
The COL pin of the PHY (U15, TLK105) is pulled down by 2.2KΩ for setting PHY address to 0x00.
But it seems that in parallel it is connected to the green LED.
According to this I believe that the voltage on this COL pin will be 3.3V - VF (RJ45 LED forward voltage).
Is it enough for resetting the address at power-up (The VIL of the TLK is 0.8V)?
2--
I can see that the green LED is also connected to RXLINK pin.
What is the functionality of this pin?
thank you
regards
Carlo