Part Number: PROCESSOR-SDK-AM437X
Other Parts Discussed in Thread: AM4378
Tool/software: Linux
Hello,
I am runing SDK 04.03.00.05 on AM437x EVM. I got failure with black screen. when toucking the Dual Camera demo in Matrix. So I run /usr/bin/dual_camera.sh I got the error message: (I installed the camera board)
root@am437x-evm:/usr/bin# ./dual_camera.sh
Stopping Matrix GUI application.
USAGE: -platform linuxfb <use_cmem flag>
Set the use_cmem flag to 1 to allocate memory from CMEM driver. By default it is set to 0
CRTCs size: 800x480
Capture 0: Opened Channel
Capture 0: Capable of streaming
Capture 0: Init done successfully
Allocating memory from OMAP DRM pool
fourcc:1448695129, fb_id 47
Allocating memory from OMAP DRM pool
fourcc:1448695129, fb_id 48
Allocating memory from OMAP DRM pool
fourcc:1448695129, fb_id 49
Capture 1: Opened Channel
Capture 1: Capable of streaming
Capture 1: Init done successfully
Allocating memory from OMAP DRM pool
fourcc:1448695129, fb_id 50
Allocating memory from OMAP DRM pool
fourcc:1448695129, fb_id 51
Allocating memory from OMAP DRM pool
fourcc:1448695129, fb_id 52
Running the demo on am437x processor
w=800, h=600
w=800, h=600
ERROR:drm_init_dss:831: ret from drmModeAtomicCommit = -13
Using Wayland-EGL
ERROR:drm_restore_props:712: ret from drmModeAtomicCommit = -13
wlpvr: PVR Services Initialised
Please help!
Thanks,
-Ken L