Hi there, I have two questions:
1) The CCS v3.3 that comes with DM6437 EVM doesn't provide the DM6437 cycle accurate simulator. I wonder if it is provided in the fully featured (and more expensive) CCS? Is the DM6437 cycle accurate simulator available?
2) For now, I'm using the C64+ cycle accurate simulator to run the profiler, especially for the L1P/L1D and L2 cache performance. I think the cache statistics is accurate, since DM6437 has a C64+ core. But I'm also concerned that the C64+ cycle accurate simulator uses a different configuration/memory map. Will this difference affect the accuracy of the cache performance as reported by the profiler?
Your timely response will be appreciated.
Thanks