Part Number: AM5728
Tool/software: Linux
Hi,
I am working the AM5728 based board. I am planning to use UART8, UART9 and UART10.
While operation, I am able to successfully transmit information from AM5728, but unable to receive the information at AM5728.
When tried to analyze, I don't have proper IRQ configured for the UART8, 9 and 10.
As per the TRM document, (Table 24-133: Interrupt Requests) I do not find mapping to any MPU_IRQ.
I need help in configuring the so that I can use it to initialize the driver properly.
Can you help me configure the UARTs ?
Thanks,
Babji.