This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Transferring RAW16 data by VPDMA

Guru 16800 points

Part Number: AM5728

Hello,

Is there any way to transfer RAW16 data from vin1a_d to DDR directly?

In 9.4.5.2 of TRM, "This 16-bit RAW input must be remapped to the RGB565 format, so that it can be saved to DDR memory properly, because the VPDMA does not support the RAW16 input format natively." is described.
However, my customers want to treat the data as RAW16 and store the data into DDR in the RAW16 format.
So, they are finding the way to avoid remapping.

Best Regards,
Nomo