Part Number: AM3358
Tool/software: Linux
I have a new custom board with the AM3358 and I need to test USB.
When I add a USB device to the bus, I do not see it show up in Linux.
I would like to check for bus activity.
Is there a way to generate USB bus activity so we can check for it on the scope from either Linux or U-Boot?
So far, I have been running this ‘usb start’ command from uboot, over and over and not seeing any activity on USB0_DP N17 or USB0_DM N18.
=> usb start starting USB... USB0: Port not available. =>
if there is a Linux command to test usb and generate bus activity, please let me know.
Thanks.