Other Parts Discussed in Thread: AM1808
Can the AM1808 source the current required to directly drive a few LEDs with GPIO? Does the I(OH)/(OL) spec of +/- 6 mA max mean that it is not really practical since most common LEDs require at least 4 or 5 mA to light, and I need to keep my current limiting resistor and Vf tolerances such that I never exceed 6 mA, or am I reading that spec wrong (section 5.3 on pg 68)?