Part Number: AM3352
Other Parts Discussed in Thread: TPS65217
When I flash am335x-shgc300.dtb, zImage, MLO, u-boot and ubi files and write to nand chip. Device boots correctly but when I reboot it again gives kernel Panic
U-Boot 2013.10-g233e888 (Jun 21 2017 - 15:01:07)
I2C: ready
DRAM: 256 MiB
NAND: 512 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - bad CRC, using default environment
Net: <ethaddr> not set. Validating first E-fuse MAC
Could not get PHY for cpsw: addr 0
cpsw, usb_ether
Standard mode
Hit any key to stop autoboot: 0
Card did not respond to voltage select!
mmc0(part 0) is current device
Scanning mmc 0...
Card did not respond to voltage select!
** Bad device mmc 0 **
Card did not respond to voltage select!
mmc0(part 0) is current device
Card did not respond to voltage select!
Card did not respond to voltage select!
mmc1(part 0) is current device
Card did not respond to voltage select!
Booting from nand ...
NAND read: device 0 offset 0x80000, size 0x40000
262144 bytes read: OK
NAND read: device 0 offset 0x200000, size 0x800000
8388608 bytes read: OK
Kernel image @ 0x80200000 [ 0x000000 - 0x3eb518 ]
## Flattened Device Tree blob at 80f80000
Booting using the fdt blob at 0x80f80000
Loading Device Tree to 8f320000, end 8f32bdd1 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 3.14.26-g2dde1c3 (yfan@scs-2-66) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #1 Wed Jun 21 14:41:24 CST 2017
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x SHGC300
[ 0.000000] cma: CMA: reserved 24 MiB at 8d800000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64512
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048 rootfstype=ubifs rootwait=1
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 224692K/260096K available (5551K kernel code, 296K rwdata, 2004K rodata, 265K init, 230K bss, 35404K reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0769054 (7557 kB)
[ 0.000000] .init : 0xc076a000 - 0xc07ac644 ( 266 kB)
[ 0.000000] .data : 0xc07ae000 - 0xc07f8160 ( 297 kB)
[ 0.000000] .bss : 0xc07f8160 - 0xc0831b80 ( 231 kB)
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000017] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956969942ns
[ 0.000042] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000357] Console: colour dummy device 80x30
[ 0.000394] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032)
[ 0.059200] pid_max: default: 32768 minimum: 301
[ 0.059324] Security Framework initialized
[ 0.059391] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.059404] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.068873] CPU: Testing write buffer coherency: ok
[ 0.069384] Setting up static identity map for 0x80572020 - 0x80572078
[ 0.070537] devtmpfs: initialized
[ 0.072763] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.081976] omap_hwmod: tptc0 using broken dt data from edma
[ 0.082081] omap_hwmod: tptc1 using broken dt data from edma
[ 0.082175] omap_hwmod: tptc2 using broken dt data from edma
[ 0.086708] omap_hwmod: debugss: _wait_target_disable failed
[ 0.143830] pinctrl core: initialized pinctrl subsystem
[ 0.145091] regulator-dummy: no parameters
[ 0.147832] NET: Registered protocol family 16
[ 0.150400] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.153602] cpuidle: using governor ladder
[ 0.153623] cpuidle: using governor menu
[ 0.162337] syscon 44e10000.control_module: regmap [mem 0x44e10000-0x44e107fb] registered
[ 0.164208] platform 49000000.edma: alias fck already exists
[ 0.164239] platform 49000000.edma: alias fck already exists
[ 0.164258] platform 49000000.edma: alias fck already exists
[ 0.165678] OMAP GPIO hardware version 0.1
[ 0.180213] omap-gpmc 50000000.gpmc: could not find pctldev for node /pinmux@44e10800/nandflash_pins_default, deferring probe
[ 0.180254] platform 50000000.gpmc: Driver omap-gpmc requests probe deferral
[ 0.184301] No ATAGs?
[ 0.184325] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.213812] bio: create slab <bio-0> at 0
[ 0.234055] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[ 0.235463] wlan-en-regulator: 1800 mV
[ 0.236007] vmmcsd_fixed: 3300 mV
[ 0.239938] vgaarb: loaded
[ 0.240602] i2c-core: driver [palmas] using legacy suspend method
[ 0.240616] i2c-core: driver [palmas] using legacy resume method
[ 0.241522] SCSI subsystem initialized
[ 0.243901] omap_i2c 44e0b000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2c0_pins, deferring probe
[ 0.243936] platform 44e0b000.i2c: Driver omap_i2c requests probe deferral
[ 0.243971] omap_i2c 4802a000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2c1_pins, deferring probe
[ 0.243990] platform 4802a000.i2c: Driver omap_i2c requests probe deferral
[ 0.244463] pps_core: LinuxPPS API ver. 1 registered
[ 0.244476] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.244644] PTP clock support registered
[ 0.247101] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.248168] Advanced Linux Sound Architecture Driver Initialized.
[ 0.250215] Switched to clocksource timer1
[ 0.274892] NET: Registered protocol family 2
[ 0.275963] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.276007] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.276044] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.276127] TCP: reno registered
[ 0.276144] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.276168] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.276404] NET: Registered protocol family 1
[ 0.276834] RPC: Registered named UNIX socket transport module.
[ 0.276850] RPC: Registered udp transport module.
[ 0.276858] RPC: Registered tcp transport module.
[ 0.276867] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.277531] hw perfevents: enabled with ARMv7 Cortex-A8 PMU driver, 5 counters available
[ 0.281194] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.494701] VFS: Disk quotas dquot_6.5.2
[ 0.494782] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.495422] NFS: Registering the id_resolver key type
[ 0.495513] Key type id_resolver registered
[ 0.495525] Key type id_legacy registered
[ 0.495573] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 0.495785] msgmni has been set to 486
[ 0.497655] NET: Registered protocol family 38
[ 0.497706] io scheduler noop registered
[ 0.497716] io scheduler deadline registered
[ 0.497744] io scheduler cfq registered (default)
[ 0.499822] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.508093] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.512092] omap_uart 44e09000.serial: no wakeirq for uart0
[ 0.512292] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 88, base_baud = 3000000) is a OMAP UART0
[ 1.180743] console [ttyO0] enabled
[ 1.185282] omap_uart 48022000.serial: no wakeirq for uart0
[ 1.191466] 48022000.serial: ttyO1 at MMIO 0x48022000 (irq = 89, base_baud = 3000000) is a OMAP UART1
[ 1.201917] omap_uart 48024000.serial: no wakeirq for uart0
[ 1.207999] 48024000.serial: ttyO2 at MMIO 0x48024000 (irq = 90, base_baud = 3000000) is a OMAP UART2
[ 1.218461] omap_uart 481a6000.serial: no wakeirq for uart0
[ 1.224587] 481a6000.serial: ttyO3 at MMIO 0x481a6000 (irq = 60, base_baud = 3000000) is a OMAP UART3
[ 1.234979] omap_uart 481a8000.serial: no wakeirq for uart0
[ 1.241093] 481a8000.serial: ttyO4 at MMIO 0x481a8000 (irq = 61, base_baud = 3000000) is a OMAP UART4
[ 1.252460] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ 1.259902] [drm] Initialized drm 1.1.0 20060810
[ 1.278643] brd: module loaded
[ 1.289021] loop: module loaded
[ 1.292874] (hci_tty): inside hci_tty_init
[ 1.297773] (hci_tty): allocated 249, 0
[ 1.305202] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.318073] mousedev: PS/2 mouse device common for all mice
[ 1.326431] i2c-core: driver [rtc-ds1307] using legacy suspend method
[ 1.333274] i2c-core: driver [rtc-ds1307] using legacy resume method
[ 1.341015] i2c /dev entries driver
[ 1.344879] Driver for 1-wire Dallas network protocol.
[ 1.353064] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.521097] pinctrl-single 44e10800.pinmux: pin 44e10978.0 already requested by 48022000.serial; cannot claim for leds.4
[ 1.532618] pinctrl-single 44e10800.pinmux: pin-94 (leds.4) status -22
[ 1.539499] pinctrl-single 44e10800.pinmux: could not request pin 94 (44e10978.0) from group user_leds_default on device pinctrl-single
[ 1.552428] leds-gpio leds.4: Error applying setting, reverse things back
[ 1.564091] omap_hsmmc 481d8000.mmc: card claims to support voltages below defined range
[ 1.574095] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.580943] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 1.588632] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 1.596836] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[ 1.608587] oprofile: using arm/armv7
[ 1.612987] TCP: cubic registered
[ 1.616496] Initializing XFRM netlink socket
[ 1.621069] NET: Registered protocol family 17
[ 1.625813] NET: Registered protocol family 15
[ 1.630679] Key type dns_resolver registered
[ 1.636668] cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
[ 1.645882] cpu cpu0: cpu0 clock notifier not ready, retry
[ 1.651722] platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
[ 1.660428] PM: could not locate rtc hwmod
[ 1.664754] ThumbEE CPU extension supported.
[ 1.669285] Registering SWP/SWPB emulation handler
[ 1.674625] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
[ 1.682520] vmmcsd_fixed: disabling
[ 1.686210] regulator-dummy: disabling
[ 1.691226] mmc1: new high speed SDIO card at address 0001
[ 1.701261] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.706691] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.714234] nand: device found, Manufacturer ID: 0x98, Chip ID: 0xdc
[ 1.720984] nand: Toshiba NAND 512MiB 3,3V 8-bit
[ 1.725847] nand: 512MiB, SLC, page size: 2048, OOB size: 128
[ 1.731911] NAND_OMAP_PREFETCH_POLLED
[ 1.735763] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
[ 1.741561] 10 ofpart partitions found on MTD device omap2-nand.0
[ 1.747983] Creating 10 MTD partitions on "omap2-nand.0":
[ 1.753699] 0x000000000000-0x000000020000 : "NAND.SPL"
[ 1.761369] 0x000000020000-0x000000040000 : "NAND.SPL.backup1"
[ 1.769417] 0x000000040000-0x000000060000 : "NAND.SPL.backup2"
[ 1.777530] 0x000000060000-0x000000080000 : "NAND.SPL.backup3"
[ 1.785664] 0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os"
[ 1.794137] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot"
[ 1.802632] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env"
[ 1.810552] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1"
[ 1.819221] 0x000000200000-0x000000a00000 : "NAND.kernel"
[ 1.833383] 0x000000a00000-0x000020000000 : "NAND.file-system"
[ 2.260202] DCDC1: at 1500 mV
[ 2.264773] vdd_mpu: 900 <--> 1225 mV at 1200 mV
[ 2.270966] vdd_core: 900 <--> 1150 mV at 1100 mV
[ 2.277176] LDO1: at 1800 mV
[ 2.281510] LDO2: at 3300 mV
[ 2.285798] LDO3: 1800 mV
[ 2.289847] LDO4: at 3300 mV
[ 2.294277] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 2.299917] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 2.309195] rtc-ds1307 1-006f: rtc core: registered mcp7941x as rtc0
[ 2.316029] rtc-ds1307 1-006f: 64 bytes nvram
[ 2.320669] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz
[ 2.327048] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[ 2.335091] cpu cpu0: of_pm_voltdm_notifier_register: Fail calculating voltage latency[950000<->1100000]:-22
[ 2.346204] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[ 2.354660] UBI: attaching mtd9 to ubi0
[ 4.820951] UBI: scanning is finished
[ 4.840397] UBI: attached mtd9 (name "NAND.file-system", size 502 MiB) to ubi0
[ 4.848019] UBI: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes
[ 4.855189] UBI: min./max. I/O unit sizes: 2048/2048, sub-page size 512
[ 4.862167] UBI: VID header offset: 2048 (aligned 2048), data offset: 4096
[ 4.869399] UBI: good PEBs: 4012, bad PEBs: 4, corrupted PEBs: 0
[ 4.875733] UBI: user volume: 1, internal volumes: 1, max. volumes count: 128
[ 4.883258] UBI: max/mean erase counter: 2/0, WL threshold: 4096, image sequence number: 0
[ 4.891972] UBI: available PEBs: 215, total reserved PEBs: 3797, PEBs reserved for bad PEB handling: 76
[ 4.901887] UBI: background thread "ubi_bgt0d" started, PID 779
[ 4.970287] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 4.976726] davinci_mdio 4a101000.mdio: detected phy mask fffffffd
[ 4.984122] libphy: 4a101000.mdio: probed
[ 4.988362] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver Atheros 8031 ethernet
[ 4.998539] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[ 5.006552] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[ 5.015084] cpsw 4a100000.ethernet: Detected MACID = 04:a3:16:b6:67:28
[ 5.022487] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[ 5.031532] cpsw 4a100000.ethernet: cpsw: Detected MACID = 04:a3:16:b6:67:2a
[ 5.040490] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[ 5.049986] input: gpio_buttons.5 as /devices/gpio_buttons.5/input/input0
[ 5.058364] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[ 5.066685] rtc-ds1307 1-006f: setting system clock to 2018-05-24 07:56:23 UTC (1527148583)
[ 5.079124] ALSA device list:
[ 5.082335] No soundcards found.
[ 5.088550] UBIFS: background thread "ubifs_bgt0_0" started, PID 795
[ 5.111512] UBI warning: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 3:4096, read only 126976 bytes, retry
[ 5.141009] UBI warning: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 3:4096, read only 126976 bytes, retry
[ 5.170485] UBI warning: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 3:4096, read only 126976 bytes, retry
[ 5.199957] UBI error: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 3:4096, read 126976 bytes
[ 5.211345] CPU: 0 PID: 1 Comm: swapper Not tainted 3.14.26-g2dde1c3 #1
[ 5.218309] Backtrace:
[ 5.220947] [<c0011268>] (dump_backtrace) from [<c0011404>] (show_stack+0x18/0x1c)
[ 5.228917] r6:cd2ae000 r5:0001f000 r4:ffffffb6 r3:00000000
[ 5.234929] [<c00113ec>] (show_stack) from [<c056a7b8>] (dump_stack+0x20/0x28)
[ 5.242564] [<c056a798>] (dump_stack) from [<c03d4b58>] (ubi_io_read+0x128/0x2ec)
[ 5.250464] [<c03d4a30>] (ubi_io_read) from [<c03d2924>] (ubi_eba_read_leb+0x134/0x3c8)
[ 5.258884] r10:00000003 r9:d093b000 r8:00000001 r7:00000000 r6:cd342800 r5:cd2ae000
[ 5.267167] r4:cd342800
[ 5.269853] [<c03d27f0>] (ubi_eba_read_leb) from [<c03d1ee8>] (ubi_leb_read+0xb0/0x124)
[ 5.278295] r10:00000001 r9:cd2f97a0 r8:00000003 r7:d093b000 r6:00000e85 r5:00000000
[ 5.286577] r4:cd342800
[ 5.289262] [<c03d1e38>] (ubi_leb_read) from [<c01f7f24>] (ubifs_leb_read+0x30/0x94)
[ 5.297430] r8:cd2f9000 r7:00000001 r6:00000000 r5:0001f000 r4:cd3f1f80
[ 5.304534] [<c01f7ef4>] (ubifs_leb_read) from [<c01ff4b4>] (ubifs_start_scan+0x78/0xec)
[ 5.313059] r7:00000001 r6:d093b000 r5:00000000 r4:cd3f1f80
[ 5.319043] [<c01ff43c>] (ubifs_start_scan) from [<c01ff7c0>] (ubifs_scan+0x30/0x350)
[ 5.327288] r8:00000001 r7:cd2f9000 r6:d093b000 r5:00000000 r4:0001f000
[ 5.334390] [<c01ff790>] (ubifs_scan) from [<c01fe88c>] (ubifs_read_master+0x48/0x8e4)
[ 5.342739] r10:00000000 r9:cd2f97a0 r8:cd2f9000 r7:00000001 r6:cd370540 r5:cd2f9000
[ 5.351026] r4:cd2fe000
[ 5.353701] [<c01fe844>] (ubifs_read_master) from [<c01f5f0c>] (ubifs_mount+0xcb4/0x15ac)
[ 5.362322] r10:00000000 r9:cd2f97a0 r8:cd2f9008 r7:cd39ca00 r6:cd370540 r5:cd2f9000
[ 5.370611] r4:cd2fe000
[ 5.373301] [<c01f5258>] (ubifs_mount) from [<c00ce314>] (mount_fs+0x4c/0x180)
[ 5.380918] r10:00000000 r9:00008000 r8:c07cd09c r7:c07cd09c r6:cd3705c0 r5:00000000
[ 5.389183] r4:00008000
[ 5.391879] [<c00ce2c8>] (mount_fs) from [<c00e50b4>] (vfs_kern_mount+0x54/0xd4)
[ 5.399669] r10:cd370600 r9:00008000 r8:00000000 r7:c07cd09c r6:00008000 r5:cd3705c0
[ 5.407953] r4:cd01f200
[ 5.410646] [<c00e5060>] (vfs_kern_mount) from [<c00e746c>] (do_mount+0x1fc/0x964)
[ 5.418619] r8:00000020 r7:cd3705c0 r6:00000000 r5:c07c5b0c r4:c07cd09c r3:00000000
[ 5.426819] [<c00e7270>] (do_mount) from [<c00e7f18>] (SyS_mount+0x8c/0xc0)
[ 5.434161] r10:c079e7c8 r9:c079e7a0 r8:cfd952e0 r7:00008000 r6:c079e7d4 r5:cd094000
[ 5.442446] r4:00000000
[ 5.445136] [<c00e7e8c>] (SyS_mount) from [<c076afc4>] (mount_block_root+0x10c/0x240)
[ 5.453394] r7:c079e7d4 r6:cd397000 r5:00008000 r4:cd397000
[ 5.459381] [<c076aeb8>] (mount_block_root) from [<c076b394>] (prepare_namespace+0x94/0x1cc)
[ 5.468279] r10:c079e7a8 r9:c079e7a0 r8:c076a4d0 r7:000000b0 r6:c07f8180 r5:c079e7d4
[ 5.476560] r4:c079e7c8
[ 5.479238] [<c076b300>] (prepare_namespace) from [<c076ac74>] (kernel_init_freeable+0x174/0x1b8)
[ 5.488580] r5:00000007 r4:c07ac598
[ 5.492389] [<c076ab00>] (kernel_init_freeable) from [<c0565834>] (kernel_init+0x14/0xf4)
[ 5.501011] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0565820
[ 5.509287] r4:c07f8180
[ 5.511980] [<c0565820>] (kernel_init) from [<c000e878>] (ret_from_fork+0x14/0x3c)
[ 5.519949] r4:00000000 r3:cd06c000
[ 5.541507] UBI warning: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 4:4096, read only 126976 bytes, retry
[ 5.571005] UBI warning: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 4:4096, read only 126976 bytes, retry
[ 5.600486] UBI warning: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 4:4096, read only 126976 bytes, retry
[ 5.629942] UBI error: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PEB 4:4096, read 126976 bytes
[ 5.641326] CPU: 0 PID: 1 Comm: swapper Not tainted 3.14.26-g2dde1c3 #1
[ 5.648282] Backtrace:
[ 5.650905] [<c0011268>] (dump_backtrace) from [<c0011404>] (show_stack+0x18/0x1c)
[ 5.658868] r6:cd2ae000 r5:0001f000 r4:ffffffb6 r3:00000000
[ 5.664881] [<c00113ec>] (show_stack) from [<c056a7b8>] (dump_stack+0x20/0x28)
[ 5.672504] [<c056a798>] (dump_stack) from [<c03d4b58>] (ubi_io_read+0x128/0x2ec)
[ 5.680407] [<c03d4a30>] (ubi_io_read) from [<c03d2924>] (ubi_eba_read_leb+0x134/0x3c8)
[ 5.688835] r10:00000004 r9:d093b000 r8:00000002 r7:00000000 r6:cd342800 r5:cd2ae000
[ 5.697118] r4:cd342800
[ 5.699798] [<c03d27f0>] (ubi_eba_read_leb) from [<c03d1ee8>] (ubi_leb_read+0xb0/0x124)
[ 5.708242] r10:00000002 r9:cd2f97a0 r8:00000003 r7:d093b000 r6:00000e85 r5:00000000
[ 5.716526] r4:cd342800
[ 5.719207] [<c03d1e38>] (ubi_leb_read) from [<c01f7f24>] (ubifs_leb_read+0x30/0x94)
[ 5.727367] r8:cd2f9000 r7:00000002 r6:00000000 r5:0001f000 r4:cd3f1f80
[ 5.734469] [<c01f7ef4>] (ubifs_leb_read) from [<c01ff4b4>] (ubifs_start_scan+0x78/0xec)
[ 5.742998] r7:00000002 r6:d093b000 r5:00000000 r4:cd3f1f80
[ 5.748981] [<c01ff43c>] (ubifs_start_scan) from [<c01ff7c0>] (ubifs_scan+0x30/0x350)
[ 5.757235] r8:00000001 r7:cd2f9000 r6:d093b000 r5:00000000 r4:0001f000
[ 5.764336] [<c01ff790>] (ubifs_scan) from [<c01fe8ec>] (ubifs_read_master+0xa8/0x8e4)
[ 5.772677] r10:00000000 r9:cd2f97a0 r8:cd2f9000 r7:00003000 r6:00000007 r5:cd3f1dc0
[ 5.780958] r4:cd3f1f80
[ 5.783638] [<c01fe844>] (ubifs_read_master) from [<c01f5f0c>] (ubifs_mount+0xcb4/0x15ac)
[ 5.792253] r10:00000000 r9:cd2f97a0 r8:cd2f9008 r7:cd39ca00 r6:cd370540 r5:cd2f9000
[ 5.800535] r4:cd2fe000
[ 5.803214] [<c01f5258>] (ubifs_mount) from [<c00ce314>] (mount_fs+0x4c/0x180)
[ 5.810828] r10:00000000 r9:00008000 r8:c07cd09c r7:c07cd09c r6:cd3705c0 r5:00000000
[ 5.819097] r4:00008000
[ 5.821804] [<c00ce2c8>] (mount_fs) from [<c00e50b4>] (vfs_kern_mount+0x54/0xd4)
[ 5.829591] r10:cd370600 r9:00008000 r8:00000000 r7:c07cd09c r6:00008000 r5:cd3705c0
[ 5.837869] r4:cd01f200
[ 5.840559] [<c00e5060>] (vfs_kern_mount) from [<c00e746c>] (do_mount+0x1fc/0x964)
[ 5.848532] r8:00000020 r7:cd3705c0 r6:00000000 r5:c07c5b0c r4:c07cd09c r3:00000000
[ 5.856733] [<c00e7270>] (do_mount) from [<c00e7f18>] (SyS_mount+0x8c/0xc0)
[ 5.864069] r10:c079e7c8 r9:c079e7a0 r8:cfd952e0 r7:00008000 r6:c079e7d4 r5:cd094000
[ 5.872352] r4:00000000
[ 5.875037] [<c00e7e8c>] (SyS_mount) from [<c076afc4>] (mount_block_root+0x10c/0x240)
[ 5.883292] r7:c079e7d4 r6:cd397000 r5:00008000 r4:cd397000
[ 5.889285] [<c076aeb8>] (mount_block_root) from [<c076b394>] (prepare_namespace+0x94/0x1cc)
[ 5.898178] r10:c079e7a8 r9:c079e7a0 r8:c076a4d0 r7:000000b0 r6:c07f8180 r5:c079e7d4
[ 5.906461] r4:c079e7c8
[ 5.909138] [<c076b300>] (prepare_namespace) from [<c076ac74>] (kernel_init_freeable+0x174/0x1b8)
[ 5.918485] r5:00000007 r4:c07ac598
[ 5.922289] [<c076ab00>] (kernel_init_freeable) from [<c0565834>] (kernel_init+0x14/0xf4)
[ 5.930910] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0565820
[ 5.939176] r4:c07f8180
[ 5.941876] [<c0565820>] (kernel_init) from [<c000e878>] (ret_from_fork+0x14/0x3c)
[ 5.949844] r4:00000000 r3:cd06c000
[ 5.954660] UBI warning: ubi_io_read: error -74 (ECC error) while reading 108 bytes from PEB 949:76072, read only 108 bytes, retry
[ 5.967429] UBI warning: ubi_io_read: error -74 (ECC error) while reading 108 bytes from PEB 949:76072, read only 108 bytes, retry
[ 5.980185] UBI warning: ubi_io_read: error -74 (ECC error) while reading 108 bytes from PEB 949:76072, read only 108 bytes, retry
[ 5.992933] UBI error: ubi_io_read: error -74 (ECC error) while reading 108 bytes from PEB 949:76072, read 108 bytes
[ 6.004034] CPU: 0 PID: 1 Comm: swapper Not tainted 3.14.26-g2dde1c3 #1
[ 6.011008] Backtrace:
[ 6.013612] [<c0011268>] (dump_backtrace) from [<c0011404>] (show_stack+0x18/0x1c)
[ 6.021597] r6:cd2ae000 r5:0000006c r4:ffffffb6 r3:00000000
[ 6.027583] [<c00113ec>] (show_stack) from [<c056a7b8>] (dump_stack+0x20/0x28)
[ 6.035211] [<c056a798>] (dump_stack) from [<c03d4b58>] (ubi_io_read+0x128/0x2ec)
[ 6.043130] [<c03d4a30>] (ubi_io_read) from [<c03d2924>] (ubi_eba_read_leb+0x134/0x3c8)
[ 6.051573] r10:000003b5 r9:cd337680 r8:000003b3 r7:00000000 r6:cd342800 r5:cd2ae000
[ 6.059847] r4:cd342800
[ 6.062544] [<c03d27f0>] (ubi_eba_read_leb) from [<c03d1ee8>] (ubi_leb_read+0xb0/0x124)
[ 6.070984] r10:cd337680 r9:00000009 r8:00000003 r7:cd337680 r6:00000e85 r5:00000000
[ 6.079256] r4:cd342800
[ 6.081949] [<c03d1e38>] (ubi_leb_read) from [<c01f7f24>] (ubifs_leb_read+0x30/0x94)
[ 6.090097] r8:0000006c r7:000003b3 r6:00011928 r5:0000006c r4:cd39c600
[ 6.097198] [<c01f7ef4>] (ubifs_leb_read) from [<c01f98f8>] (ubifs_read_node+0xa0/0x284)
[ 6.105730] r7:000003b3 r6:cd2f9000 r5:00011928 r4:cd39c600
[ 6.111739] [<c01f9858>] (ubifs_read_node) from [<c02021f0>] (dbg_old_index_check_init+0x6c/0xac)
[ 6.121093] r10:0000006c r9:00000800 r8:000003b3 r7:00011928 r6:cd2f9000 r5:cd337680
[ 6.129368] r4:cd39c600
[ 6.132062] [<c0202184>] (dbg_old_index_check_init) from [<c01fef2c>] (ubifs_read_master+0x6e8/0x8e4)
[ 6.141775] r10:00000000 r8:cd2f9000 r7:00000000 r6:00000000 r5:00000000 r4:150eb740
[ 6.150056] [<c01fe844>] (ubifs_read_master) from [<c01f5f0c>] (ubifs_mount+0xcb4/0x15ac)
[ 6.158678] r10:00000000 r9:cd2f97a0 r8:cd2f9008 r7:cd39ca00 r6:cd370540 r5:cd2f9000
[ 6.166956] r4:cd2fe000
[ 6.169637] [<c01f5258>] (ubifs_mount) from [<c00ce314>] (mount_fs+0x4c/0x180)
[ 6.177245] r10:00000000 r9:00008000 r8:c07cd09c r7:c07cd09c r6:cd3705c0 r5:00000000
[ 6.185528] r4:00008000
[ 6.188203] [<c00ce2c8>] (mount_fs) from [<c00e50b4>] (vfs_kern_mount+0x54/0xd4)
[ 6.196000] r10:cd370600 r9:00008000 r8:00000000 r7:c07cd09c r6:00008000 r5:cd3705c0
[ 6.204285] r4:cd01f200
[ 6.206964] [<c00e5060>] (vfs_kern_mount) from [<c00e746c>] (do_mount+0x1fc/0x964)
[ 6.214945] r8:00000020 r7:cd3705c0 r6:00000000 r5:c07c5b0c r4:c07cd09c r3:00000000
[ 6.223150] [<c00e7270>] (do_mount) from [<c00e7f18>] (SyS_mount+0x8c/0xc0)
[ 6.230489] r10:c079e7c8 r9:c079e7a0 r8:cfd952e0 r7:00008000 r6:c079e7d4 r5:cd094000
[ 6.238755] r4:00000000
[ 6.241452] [<c00e7e8c>] (SyS_mount) from [<c076afc4>] (mount_block_root+0x10c/0x240)
[ 6.249693] r7:c079e7d4 r6:cd397000 r5:00008000 r4:cd397000
[ 6.255697] [<c076aeb8>] (mount_block_root) from [<c076b394>] (prepare_namespace+0x94/0x1cc)
[ 6.264598] r10:c079e7a8 r9:c079e7a0 r8:c076a4d0 r7:000000b0 r6:c07f8180 r5:c079e7d4
[ 6.272881] r4:c079e7c8
[ 6.275560] [<c076b300>] (prepare_namespace) from [<c076ac74>] (kernel_init_freeable+0x174/0x1b8)
[ 6.284911] r5:00000007 r4:c07ac598
[ 6.288695] [<c076ab00>] (kernel_init_freeable) from [<c0565834>] (kernel_init+0x14/0xf4)
[ 6.297316] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0565820
[ 6.305600] r4:c07f8180
[ 6.308277] [<c0565820>] (kernel_init) from [<c000e878>] (ret_from_fork+0x14/0x3c)
[ 6.316261] r4:00000000 r3:cd06c000
[ 6.320809] UBI warning: ubi_io_read: error -74 (ECC error) while reading 11 bytes from PEB 10:16384, read only 11 bytes, retry
[ 6.333313] UBI warning: ubi_io_read: error -74 (ECC error) while reading 11 bytes from PEB 10:16384, read only 11 bytes, retry
[ 6.345776] UBI warning: ubi_io_read: error -74 (ECC error) while reading 11 bytes from PEB 10:16384, read only 11 bytes, retry
[ 6.358241] UBI error: ubi_io_read: error -74 (ECC error) while reading 11 bytes from PEB 10:16384, read 11 bytes
[ 6.369060] CPU: 0 PID: 1 Comm: swapper Not tainted 3.14.26-g2dde1c3 #1
[ 6.376036] Backtrace:
[ 6.378640] [<c0011268>] (dump_backtrace) from [<c0011404>] (show_stack+0x18/0x1c)
[ 6.386621] r6:cd2ae000 r5:0000000b r4:ffffffb6 r3:00000000
[ 6.392623] [<c00113ec>] (show_stack) from [<c056a7b8>] (dump_stack+0x20/0x28)
[ 6.400253] [<c056a798>] (dump_stack) from [<c03d4b58>] (ubi_io_read+0x128/0x2ec)
[ 6.408137] [<c03d4a30>] (ubi_io_read) from [<c03d2924>] (ubi_eba_read_leb+0x134/0x3c8)
[ 6.416569] r10:0000000a r9:d097d000 r8:00000008 r7:00000000 r6:cd342800 r5:cd2ae000
[ 6.424854] r4:cd342800
[ 6.427532] [<c03d27f0>] (ubi_eba_read_leb) from [<c03d1ee8>] (ubi_leb_read+0xb0/0x124)
[ 6.435962] r10:00000003 r9:d097d000 r8:00000003 r7:d097d000 r6:00000e85 r5:00000000
[ 6.444239] r4:cd342800
[ 6.446917] [<c03d1e38>] (ubi_leb_read) from [<c01f7f24>] (ubifs_leb_read+0x30/0x94)
[ 6.455083] r8:c0810b7c r7:00000008 r6:00003000 r5:0000000b r4:cd2f9000
[ 6.462191] [<c01f7ef4>] (ubifs_leb_read) from [<c020c360>] (ubifs_lpt_init+0x250/0x498)
[ 6.470718] r7:00000001 r6:00000001 r5:cd2f9024 r4:cd2f9000
[ 6.476705] [<c020c110>] (ubifs_lpt_init) from [<c01f5fd8>] (ubifs_mount+0xd80/0x15ac)
[ 6.485046] r10:00000e7a r9:00000000 r8:0001e5a0 r7:cd39ca00 r6:cd370540 r5:cd2f9000
[ 6.493324] r4:000008f8
[ 6.496005] [<c01f5258>] (ubifs_mount) from [<c00ce314>] (mount_fs+0x4c/0x180)
[ 6.503615] r10:00000000 r9:00008000 r8:c07cd09c r7:c07cd09c r6:cd3705c0 r5:00000000
[ 6.511901] r4:00008000
[ 6.514578] [<c00ce2c8>] (mount_fs) from [<c00e50b4>] (vfs_kern_mount+0x54/0xd4)
[ 6.522376] r10:cd370600 r9:00008000 r8:00000000 r7:c07cd09c r6:00008000 r5:cd3705c0
[ 6.530653] r4:cd01f200
[ 6.533332] [<c00e5060>] (vfs_kern_mount) from [<c00e746c>] (do_mount+0x1fc/0x964)
[ 6.541316] r8:00000020 r7:cd3705c0 r6:00000000 r5:c07c5b0c r4:c07cd09c r3:00000000
[ 6.549501] [<c00e7270>] (do_mount) from [<c00e7f18>] (SyS_mount+0x8c/0xc0)
[ 6.556837] r10:c079e7c8 r9:c079e7a0 r8:cfd952e0 r7:00008000 r6:c079e7d4 r5:cd094000
[ 6.565116] r4:00000000
[ 6.567796] [<c00e7e8c>] (SyS_mount) from [<c076afc4>] (mount_block_root+0x10c/0x240)
[ 6.576054] r7:c079e7d4 r6:cd397000 r5:00008000 r4:cd397000
[ 6.582054] [<c076aeb8>] (mount_block_root) from [<c076b394>] (prepare_namespace+0x94/0x1cc)
[ 6.590938] r10:c079e7a8 r9:c079e7a0 r8:c076a4d0 r7:000000b0 r6:c07f8180 r5:c079e7d4
[ 6.599209] r4:c079e7c8
[ 6.601898] [<c076b300>] (prepare_namespace) from [<c076ac74>] (kernel_init_freeable+0x174/0x1b8)
[ 6.611247] r5:00000007 r4:c07ac598
[ 6.615033] [<c076ab00>] (kernel_init_freeable) from [<c0565834>] (kernel_init+0x14/0xf4)
[ 6.623662] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0565820
[ 6.631950] r4:c07f8180
[ 6.634631] [<c0565820>] (kernel_init) from [<c000e878>] (ret_from_fork+0x14/0x3c)
[ 6.642605] r4:00000000 r3:cd06c000
[ 6.646383] UBIFS error (pid 1): ubifs_leb_read: reading 11 bytes from LEB 8:12288 failed, error -74
[ 6.656012] CPU: 0 PID: 1 Comm: swapper Not tainted 3.14.26-g2dde1c3 #1
[ 6.662980] Backtrace:
[ 6.665569] [<c0011268>] (dump_backtrace) from [<c0011404>] (show_stack+0x18/0x1c)
[ 6.673549] r6:00003000 r5:0000000b r4:ffffffb6 r3:00000000
[ 6.679539] [<c00113ec>] (show_stack) from [<c056a7b8>] (dump_stack+0x20/0x28)
[ 6.687157] [<c056a798>] (dump_stack) from [<c01f7f7c>] (ubifs_leb_read+0x88/0x94)
[ 6.695141] [<c01f7ef4>] (ubifs_leb_read) from [<c020c360>] (ubifs_lpt_init+0x250/0x498)
[ 6.703666] r7:00000001 r6:00000001 r5:cd2f9024 r4:cd2f9000
[ 6.709650] [<c020c110>] (ubifs_lpt_init) from [<c01f5fd8>] (ubifs_mount+0xd80/0x15ac)
[ 6.717990] r10:00000e7a r9:00000000 r8:0001e5a0 r7:cd39ca00 r6:cd370540 r5:cd2f9000
[ 6.726269] r4:000008f8
[ 6.728947] [<c01f5258>] (ubifs_mount) from [<c00ce314>] (mount_fs+0x4c/0x180)
[ 6.736554] r10:00000000 r9:00008000 r8:c07cd09c r7:c07cd09c r6:cd3705c0 r5:00000000
[ 6.744844] r4:00008000
[ 6.747523] [<c00ce2c8>] (mount_fs) from [<c00e50b4>] (vfs_kern_mount+0x54/0xd4)
[ 6.755318] r10:cd370600 r9:00008000 r8:00000000 r7:c07cd09c r6:00008000 r5:cd3705c0
[ 6.763607] r4:cd01f200
[ 6.766277] [<c00e5060>] (vfs_kern_mount) from [<c00e746c>] (do_mount+0x1fc/0x964)
[ 6.774259] r8:00000020 r7:cd3705c0 r6:00000000 r5:c07c5b0c r4:c07cd09c r3:00000000
[ 6.782460] [<c00e7270>] (do_mount) from [<c00e7f18>] (SyS_mount+0x8c/0xc0)
[ 6.789788] r10:c079e7c8 r9:c079e7a0 r8:cfd952e0 r7:00008000 r6:c079e7d4 r5:cd094000
[ 6.798074] r4:00000000
[ 6.800766] [<c00e7e8c>] (SyS_mount) from [<c076afc4>] (mount_block_root+0x10c/0x240)
[ 6.809008] r7:c079e7d4 r6:cd397000 r5:00008000 r4:cd397000
[ 6.815010] [<c076aeb8>] (mount_block_root) from [<c076b394>] (prepare_namespace+0x94/0x1cc)
[ 6.823894] r10:c079e7a8 r9:c079e7a0 r8:c076a4d0 r7:000000b0 r6:c07f8180 r5:c079e7d4
[ 6.832173] r4:c079e7c8
[ 6.834853] [<c076b300>] (prepare_namespace) from [<c076ac74>] (kernel_init_freeable+0x174/0x1b8)
[ 6.844202] r5:00000007 r4:c07ac598
[ 6.847988] [<c076ab00>] (kernel_init_freeable) from [<c0565834>] (kernel_init+0x14/0xf4)
[ 6.856608] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0565820
[ 6.864888] r4:c07f8180
[ 6.867566] [<c0565820>] (kernel_init) from [<c000e878>] (ret_from_fork+0x14/0x3c)
[ 6.875549] r4:00000000 r3:cd06c000
[ 6.879384] UBIFS: background thread "ubifs_bgt0_0" stops
[ 6.885838] VFS: Cannot open root device "ubi0:rootfs" or unknown-block(0,0): error -74
[ 6.894319] Please append a correct "root=" boot option; here are the available partitions:
[ 6.903162] 1f00 128 mtdblock0 (driver?)
[ 6.908493] 1f01 128 mtdblock1 (driver?)
[ 6.913836] 1f02 128 mtdblock2 (driver?)
[ 6.919159] 1f03 128 mtdblock3 (driver?)
[ 6.924496] 1f04 256 mtdblock4 (driver?)
[ 6.929822] 1f05 1024 mtdblock5 (driver?)
[ 6.935160] 1f06 128 mtdblock6 (driver?)
[ 6.940500] 1f07 128 mtdblock7 (driver?)
[ 6.945824] 1f08 8192 mtdblock8 (driver?)
[ 6.951164] 1f09 514048 mtdblock9 (driver?)
[ 6.956490] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)