Part Number: EVMK2H
Tool/software: TI-RTOS
My program is run on ARM cores and sending is ok over the UART(uart1).
But, I can't read a 0xff byte.
Other bytes (0x00 ~ 0xFE) is read.
I used blocking mode, callback mode and polling mode and all mode don't read a 0xff byte.
PDK version is 4.0.9 .
My settings are as follows
UART_Params_init(&uartParams1)
uartParams1.dataLength = UART_LEN_8;
uartParams1.stopBits = UART_STOP_ONE;
uartParams1.parityType = UART_PAR_NONE;
uartParams1.baudRate = 57600;
uartParams1.writeDataMode = UART_DATA_BINARY;
uartParams1.readDataMode = UART_DATA_BINARY;
uartParams1.readEcho = UART_ECHO_OFF;
uartParams1.readReturnMode = UART_RETURN_FULL;
uartParams1.readMode = UART_MODE_CALLBACK;
uartParams1.writeMode = UART_MODE_CALLBACK;
Thanks.