This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

the problems about compiling qt-embedded-linux-opensource-4.4.3

arm_v5t_le-g++ -c -pipe -O2 -Wall -W -D_REENTRANT -D_LARGEFILE64_SOURCE -D_LARGEFILE_SOURCE -DQT_NO_DEBUG -DQT_GUI_LIB -DQT_NETWORK_LIB -DQT_CORE_LIB -DQT_SHARED -I../../../mkspecs/qws/arm_v5t_le-g++ -I. -I../../../include/QtCore -I../../../include/QtCore -I../../../include/QtNetwork -I../../../include/QtNetwork -I../../../include/QtGui -I../../../include/QtGui -I../../../include -I.moc/release-shared-emb-arm -I.uic/release-shared-emb-arm -o .obj/release-shared-emb-arm/moc_screenshot.o .moc/release-shared-emb-arm/moc_screenshot.cpp
arm_v5t_le-g++ -Wl,-rpath,/usr/local/Trolltech/QtEmbedded-4.4.3-arm/lib -Wl,-rpath,/usr/local/Trolltech/QtEmbedded-4.4.3-arm/lib -o screenshot .obj/release-shared-emb-arm/main.o .obj/release-shared-emb-arm/screenshot.o .obj/release-shared-emb-arm/moc_screenshot.o    -L/mydocument/qt/qt-embedded-linux-opensource-src-4.4.3/lib -lQtGui -L/mydocument/qt/qt-embedded-linux-opensource-src-4.4.3/lib -lts -lpng -lQtNetwork -lQtCore -lm -ldl -lpthread
/mydocument/qt/qt-embedded-linux-opensource-src-4.4.3/lib/libQtCore.so: undefined reference to `QInotifyFileSystemWatcherEngine::create()'
/mydocument/qt/qt-embedded-linux-opensource-src-4.4.3/lib/libQtCore.so: undefined reference to `clock_gettime'
/mydocument/qt/qt-embedded-linux-opensource-src-4.4.3/lib/libQtCore.so: undefined reference to `QDnotifyFileSystemWatcherEngine::create()'
collect2: ld return 1
gmake[3]: *** [screenshot] error 1
gmake[3]: Leaving directory `/mydocument/qt/qt-embedded-linux-opensource-src-4.4.3/examples/desktop/screenshot'
gmake[2]: *** [sub-screenshot-make_default-ordered] error 2
gmake[2]: Leaving directory `/mydocument/qt/qt-embedded-linux-opensource-src-4.4.3/examples/desktop'
gmake[1]: *** [sub-desktop-make_default] error 2
gmake[1]: Leaving directory `/mydocument/qt/qt-embedded-linux-opensource-src-4.4.3/examples'
gmake: *** [sub-examples-make_default-ordered] error 2
[root@dengyongchao qt-embedded-linux-opensource-src-4.4.3]#

*****************************************************************************

Can i compiling qt with arm_v5t_le-g?