in document "TMS320C6472/TMS320TCI648x DSPDDR2 Memory Controller", it ssys that "device has the following configuration":
• Maximum data rate: 533MHz
• Number of banks: 8
• Page size: 1024 words
• CAS latency: 4
especially that "Maximum data rate: 533MHz",does it say that C6472 support DDR2 400 for instance,but the maxmium is 533?
If so, how should i select a DDR2 400 device,and how should i set the configuration?