This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467 video output support range



Hi,

 

Does DM6467 able to give 1280X800@60Hz resolution output on its video port ?

 

Thanks,

Hitesh

  • Hitesh,

    It should be OK. Please keep in mind DM6467 only outputs embedded sync, and if you are using DM6467 (which has a max pixel clock up to 75MHz), not DM6467T (which has a max pixel clock up to 150MHz), you will need the 16-bit Y/C non-muxed mode.