This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/LINUXSDK-OMAPL138: Having trouble rebuilding the rootfs for the sdk 4.00.00.04

Part Number: LINUXSDK-OMAPL138
Other Parts Discussed in Thread: OMAPL138, OMAP-L138

Tool/software: Linux

Hi All,

I'm trying to rebuild the SDK root filesystem,  and I think I've followed the instructions and things seem to start off pretty well,  but I get stuck during the do_install  portion of the build with a message that cp can't stat ldconfig.   It seems like I'm missing an environment variable or something.    I've attached the log with the error highlighted.   Any help is appreciated !

Thanks

Jim 

$ ./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-04.00.00.04-config.txt
$ cd build
$ . conf/setenv
$  export PATH=/home/jim/ti-processor-sdk-linux-omapl138-lcdk-04.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/bin:$PATH

 

$ MACHINE=omapl138-lcdk bitbake arago-core-tisdk-image

.

.

.

ERROR: external-linaro-toolchain-2016.11-r0.arago35.tisdk0 do_install: Function failed: do_install (log file is located at /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/temp/log.do_install.123922)

ERROR: Logfile of failure stored in: /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/temp/log.do_install.123922

Log data follows:

| DEBUG: Executing shell function do_install

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libanl.so.1 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libanl-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libBrokenLocale.so.1 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libBrokenLocale-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libc.so.6 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libc-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libcidn.so.1 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libcidn-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libcrypt.so.1 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libcrypt-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libdl.so.2 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libdl-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libm.so.6 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libm-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnsl.so.1 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnsl-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_compat.so.2 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_compat-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_db.so.2 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_db-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_dns.so.2 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_dns-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_files.so.2 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_files-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_hesiod.so.2 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_hesiod-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_nis.so.2 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_nis-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_nisplus.so.2 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libnss_nisplus-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libpthread.so.0 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libpthread-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libresolv.so.2 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libresolv-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/librt.so.1 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/librt-2.23.so, keep it

| /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libutil.so.1 is a symlink of /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/lib/libutil-2.23.so, keep it

| cp: cannot stat ‘/home/jim/ti-processor-sdk-linux-omapl138-lcdk-04.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/arm-linux-gnueabi/libc//sbin/ldconfig’: No such file or directory

| WARNING: /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/temp/run.do_install.123922:1 exit 1 from 'cp -a /home/jim/ti-processor-sdk-linux-omapl138-lcdk-04.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/arm-linux-gnueabi/libc//sbin/ldconfig /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/image/sbin/'

| ERROR: Function failed: do_install (log file is located at /home/jim/tibuild/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv5e-linux-gnueabi/external-linaro-toolchain/2016.11-r0.arago35.tisdk0/temp/log.do_install.123922)

ERROR: Task (/home/jim/tibuild/tisdk/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/external-linaro-toolchain/external-linaro-toolchain.bb:do_install) failed with exit code '1'