This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5517: C5517 I2S configuration problem

Part Number: TMS320C5517

Dear TI:

Currently debugging I2S-related interfaces, using the c55_csl_3.08\ccs_v6.x_examples\i2s\CSL_I2S_DMAExample routines, master mode FS/clk nothing out, switch I2S0 to I2 FS/CLK waveform out (switch to I2S3 nor Waveform comes out, I need to use how to set this group of I2S;


I set the main frequency is 200MHZ, hwConfig.clkDiv = I2S_CLKDIV4/hwConfig.fsDiv = I2S_FSDIV32; I2S2 when I measured clk = 50M, fs = 1.56m; how is this calculated?


Where can I download detailed information about the C5517 I2S?

Thanks!