Other Parts Discussed in Thread: TMS320F28335, TMS320C6747, OMAP-L137
I've had great success building and running the "Example DSPLIB/DSPLink" Application on OMAP-L1x on a Linux host workstation.
I'm hoping it can also support our other Inter Processor Communication needs on a TMS320F28335 connected
through the external XINT/HPI Host Port interface to a TMS320C6747. I understand that the DSPLink can be ported to
other devices and even Linux, WinCE and ProOS. ... DSPLINK FAQ
Attempting to download the DSPLink package I was confused by the 2 options Linux or 'porting kit for WinCE and ProOS'
C2000 tools are not available for Linux hosts currently only CCS so the porting kit may be appropriate. though we have no plans for
a third party OS currently.
Does DSPBios Link require a running OS on both GPP and DSP? or is it possible to run the GPP as a simple microcontroller
while(1) schedule loop? Perhaps I don't need DSPLink to implement shared memory in this case DSP/BIOS supports this without
the need for BIOS Link?
Michael Nolin