Part Number: PROCESSOR-SDK-AM437X
Other Parts Discussed in Thread: AM4378
Tool/software: Linux
I'm designing a board with the AM4378. We started designing based on the AM437x Starterkit and are currently using Linux SDK 4.3.0.5 with a build of the core image. I can't seem to find a working procedure to remove the ethernet connection on 'eth0' (RGMII1) and just use 'eth1' (RGMII2). I followed the steps from the post: http://e2e.ti.com/support/arm/sitara_arm/f/791/t/391961 which made the linux image only see one ethernet connection (eth0) but both ports on the starterkit remained active. Only 'eth0' showed up when I ran ifconfig, but 'eth0' was assigned an IP address regardless of the port I plugged the cable into. For our application we have to use some of the pins associated with RGMII1 for eMMC on MMC1 since that is the only bootable pinout for MMC1 so I have to be able to dissociate those pins from RGMII1.
The section of the devicetree that appears to be relevant is: (starterkit settings)
&mac {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
dual_emac = <2>;
status = "okay";
};
&davinci_mdio {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
status = "okay";
};
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <4>;
phy-mode = "rgmii";
dual_emac_res_vlan = <1>;
};
&cpsw_emac1 {
phy_id = <&davinci_mdio>, <5>;
phy-mode = "rgmii";
dual_emac_res_vlan = <2>;
};
The settings I tried following the recommendations in the previously linked post resulted in this section in the file am437x-sk-evm.dts:
&mac {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
status = "okay";
};
&davinci_mdio {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
status = "okay";
};
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <4>;
phy-mode = "rgmii";
};
&cpsw_emac1 {
phy_id = <&davinci_mdio>, <5>;
phy-mode = "rgmii";
};
I've also tried reversing the pin order in the cpsw section of the pinmux
What I want, but what I'm clearly not coding correctly is something like:
&mac {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
status = "okay";
};
&davinci_mdio {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
status = "okay";
};
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <5>;
phy-mode = "rgmii";
}