Hello everyone.
I'm developing Some Computer Vision Program using TIOVX on am5728.
I'm using ti-processor-sdk-linux-rt-arm57xx-evm-04.03.00.05.
And i've build OpenVX test program using TIOVX.
It's ok but when i add over 24 user kernels, 4 kernels after 20th kernels publishing failed.
Kernel Enums are like following.
#define VX_LIBRARY_PORCV 0x01
enum custome_kernel_e {
KERNEL1 = VX_KERNEL_BASE(VX_ID_DEFAULT, VX_LIBRARY_PORCV) + 0x0,
..
KERNEL20,
KERNEL21,
KERNEL22,
KERNEL23,
KERNEL24
};
from KERNEL21 to KERNEL24 publishing are failed.
if remove KERNEL20 then from KERNEL22 to KERNEL24 publishing are failed.
Does anyone know this is why?
Please help me!.
Best regards.
Thanks.