This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BIOS

Hi, everyone !

 I have a question about the prog and the bios.

 In the file: all.tcf, we see that:

prog.module("GBL").C64PLUSMAR128to159 = 0x0000FFFF;

prog.module("GBL").C64PLUSL1PCFG = "4K";

prog.module("MEM").STACKSIZE = 0x1000;

Also:

bios.DDR2.createheap = true;

First question:

I know that the "GBL" and the "MEM" are the name of the modules. But I don't know where we use them.

Second question:

What's the meaning of the "C64PLUSMAR128to159"?

C64PLUSL1PCFG maybe set the size of the L1P cache becauseof the L1PCFG, but the meaning of the C649LUS??

Third question:

 I know that the bios is refer to the Module and Instance objects.

But here the bios in  bios.DDR2.createheap is refer to which module because we define two modules---- GBL and MEM

Thank you !!