I've bought a C5515 Fingerprint development kit recently. And I have successfully connected my emulator to the target board in CCS4.1.2.0027,but I can't load the file(boot_atw.bin, boot_cmos.bin) to the spi flash of the FDK. When I follow the instruction of "C5515 FDK Software User Guide", it turns out the problem as follows:
WRITE ERROR! at 0x00008000
Wrote 0x09aa Read 0x0182
Is there anyone can help me?
Thank you!