This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Make runtest failed



Caffe jacinto build failed. Details are given below-

make runtest

Please suggest solution.

GPU : Tesla K20c

OS: Ubuntu 16.04 64bit

Error:

make runtest
.build_release/tools/caffe
I0605 16:20:30.894817 3694 caffe.cpp:807] This is NVCaffe 0.16.4 started at Tue Jun 5 16:20:30 2018
I0605 16:20:30.895033 3694 caffe.cpp:810] CuDNN version: 6021
I0605 16:20:30.895043 3694 caffe.cpp:811] CuBLAS version: 8000
I0605 16:20:30.895050 3694 caffe.cpp:812] CUDA version: 8000
I0605 16:20:30.895058 3694 caffe.cpp:813] CUDA driver version: 9000
caffe: command line brew
usage: caffe

commands:
train train or finetune a model
test score a model
device_query show GPU diagnostic information
time benchmark model execution time

Flags from tools/caffe.cpp:
-ap_version (Average Precision type for object detection) type: string
default: "11point"
-display_sparsity (Display the amount of sparsity) type: bool
default: false
-gpu (Optional; run in GPU mode on given device IDs separated by ', '.Use
'-gpu all' to run on all available GPUs. The effective training batch
size is multiplied by the number of devices.) type: string default: ""
-iterations (The number of iterations to run.) type: int32 default: 50
-model (The model definition protocol buffer text file.) type: string
default: ""
-output (Prefix for output prototxt and caffemodel) type: string
default: ""
-show_per_class_result (Show per class result for object detection)
type: bool default: true
-sighup_effect (Optional; action to take when a SIGHUP signal is received:
snapshot, stop or none.) type: string default: "snapshot"
-sigint_effect (Optional; action to take when a SIGINT signal is received:
snapshot, stop or none.) type: string default: "stop"
-snapshot (Optional; the snapshot solver state to resume training.)
type: string default: ""
-solver (The solver definition protocol buffer text file.) type: string
default: ""
-threshold_fraction_high (Optional: fraction of weights to be zeroed)
type: double default: 0.90000000000000002
-threshold_fraction_low (Optional: fraction of weights to be zeroed)
type: double default: 0.40000000000000002
-threshold_fraction_mid (Optional: fraction of weights to be zeroed)
type: double default: 0.80000000000000004
-threshold_step_factor (Optional: step factor to find the optimal threshold
for each layer) type: double default: 1e-08
-threshold_value_max (Optional: vlues of weights below which are zeroed)
type: double default: 0.0001
-threshold_value_maxratio (Optional: determine threshold as a factor of
max) type: double default: 0.001
-weights (Optional; the pretrained weights to initialize finetuning,
separated by ', '. Cannot be set simultaneously with snapshot.)
type: string default: ""
.build_release/test/test_all.testbin 0 --gtest_shuffle
Cuda number of devices: 1
Setting to use device 0
Current device id: 0
Current device name: Tesla K20c
Note: Randomizing tests' orders with a seed of 77198 .
[==========] Running 1906 tests from 266 test cases.
[----------] Global test environment set-up.
[----------] 4 tests from SoftmaxWithLossLayerTest/3, where TypeParam = caffe::GPUDevice
[ RUN ] SoftmaxWithLossLayerTest/3.TestGradient
F0605 16:20:32.456480 3715 math_functions.cu:508] Check failed: error == cudaSuccess (8 vs. 0) invalid device function
*** Check failure stack trace: ***
@ 0x7fe4fff8c5cd google::LogMessage::Fail()
@ 0x7fe4fff8e433 google::LogMessage::SendToLog()
@ 0x7fe4fff8c15b google::LogMessage::Flush()
@ 0x7fe4fff8ee1e google::LogMessageFatal::~LogMessageFatal()
@ 0x7fe4fdef85d2 caffe::caffe_gpu_set<>()
@ 0x7fe4fda95c9d caffe::Tensor::gpu_set()
@ 0x7fe4fda95eb0 caffe::Tensor::set()
@ 0x4bea78 caffe::Layer<>::SetLossWeights()
@ 0x7fe4fde45249 caffe::SoftmaxWithLossLayer<>::LayerSetUp()
@ 0x4bb0a5 caffe::LayerBase::SetUp()
@ 0x4df53f caffe::GradientChecker<>::CheckGradientExhaustive()
@ 0x5f5ccc caffe::SoftmaxWithLossLayerTest_TestGradient_Test<>::TestBody()
@ 0x86e3a3 testing::internal::HandleExceptionsInMethodIfSupported<>()
@ 0x867d1a testing::Test::Run()
@ 0x867e68 testing::TestInfo::Run()
@ 0x867f45 testing::TestCase::Run()
@ 0x8681ff testing::internal::UnitTestImpl::RunAllTests()
@ 0x868533 testing::UnitTest::Run()
@ 0x46b909 main
@ 0x7fe4fcb2f830 __libc_start_main
@ 0x475329 _start
@ (nil) (unknown)
Makefile:565: recipe for target 'runtest' failed
make: *** [runtest] Aborted (core dumped)