Part Number: TDA2EVM5777
Hello,
I am using pre-imported ssd object detection model given in TIDL Test app.
Setup :
1. TDA2x EVM Board is connected to CCS using XDS560 JTAG.
2. Build and generated eve_test_dl_algo.out and dsp_test_dl_algo.out (release mode) for test app (in tidl folder)
3. Using CCS, Load Program : eve_test_dl_algo.out executed on EVE or dsp_test_dl_algo.out executed on DSP
First Experiment:
I ran full model on EVE, with layersGroupId = 1 runFullNet = 1
Second Experiment:
I ran full model on DSP, with layersGroupId = 2 runFullNet = 1
Third Experiment:
I ran only EVE part model, with layersGroupId = 1 runFullNet = 0
Fourth Experiment:
I ran only DSP part model, with layersGroupId = 2 runFullNet = 0
I have attached 4 logs and 4 infer config files for each experiment. PFA
DSP Freq: 600 MHZ
EVE Freq: 535 MHz
Queries :
1. Execution Time:
| Full EVE | 1553601318 | 2.903 seconds |
| Full DSP | 951400000 | 1.585 seconds |
|
Part EVE |
103899088 | 0.194 seconds |
| Part DSP | 4164380000 | 6.940 seconds |
What is the expected execution time? According to datasheet EVE Part Execution takes 93.69 Mega Cycles and DSP Part Execution takes 13.01 Mega Cycles.
Total Execution Time: 175 ms + 0.021 seconds = ~ 0.2 seconds
Can you comment on execution time that i have calculated from the above experiment?
2. How to execute Part DSP ?
- Part DSP execution time is very high, and from the log we can see most of the cycles are consumed by DetectionOutput Layer
- Please check the infer config file part dsp execution which i have attached.
3. If i am comparing TSC Cycles for each layer of EVE Full Execution (Layer 0 to Layer 43) and EVE Part Execution (Layer 0 to Layer 39), are matching. But, Same for DSP Full Execution (Layer 0 to Layer 43) and DSP Part Execution (Layer 22 to Layer 43) are not matching
- Please comment on this
4. Obj Release vs Source Release
- I am observing different TSC Cycles for the same input models for test app using obj release Algo and test app using source release Algo
- Test App from REL.TIDLSRC.01.01.00.00 and Test App from REL.TIDL.01.01.00.00
- Can you share information about How to build Algo Libs from source release (Important Flags/Macros to disable or enable) for board?
- Size of the eve release algo lib built by me from sources is (tidl_algo.lib) 3051 KB whereas default obj release size is (tidl_algo.lib) 2748 KB
Regards,
Sagar