This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem in ethernet transmission using dm6437 dvdp

Other Parts Discussed in Thread: TMS320DM6437

i am trying to send video over ethernet  using the tms320dm6437 dvdp from board to the PC.

For capturing and encoding the video i have used video_encdec.pjt(from dvsdk) and for ethernet emac.pjt given by TI.

I send the h.264 encoded video buffer to the following code

"iCount" is the no. of packets which varies with each frame size.

The packet_data[0] to packet_data[15] is the header part

*************************************************

 for (i=0 ; i<iCount; i++)/////
    { 
      ptr = & packet_data[16];
  memcpy(ptr, encoded1 + TX_SIZE * i,TX_SIZE);
  
     pDesc            = pDescBase + 1;
     pDesc->pNext     = 0;////////
     pDesc->pBuffer   = packet_data;
     pDesc->BufOffLen = 1514;
     pDesc->PktFlgLen = EMAC_DSC_FLAG_OWNER
                     | EMAC_DSC_FLAG_SOP
                     | EMAC_DSC_FLAG_EOP
                     | 1514;

     pDescTx = pDescBase + 1;
    EMAC_TX0HDP = ( Uint32 )pDescTx;

        /* Busy period */
    _wait( 10000 );

    /* Manually check ISR, if using interrupts this will be done automatically */
    EMAC_isr( );
}

**********************************************

But for each frame i am getting the same data in every packet and this data corresponds to the data of the last packet of previous frame. So for the first frame i get the data which was present previously (i.e. before running) in the "packet_data".

Same thing happens for raw data also...

Thankyou in advance 

  • Rutcha,

    I assume that you are trying to transmit TX_SIZE bytes of data, but the packet descriptors are telling EMAC to transmit 1514 bytes.  Is TX_SIZE equal to 1514?

     

    -Michael

  • hi....

    no TX_SIZE = 1498 i.e. 1514-16 bytes of header. so each packet contains 1498 bytes of data.

  • Rutcha,

    The packet size that you program into the descriptors should include some header-type data bytes like DST ADDR, SRC ADDR, and LEN.  Please ensure that this is handled in the program.  You can see a figure of the frame in Section 2.4.1 of the EMAC user guide (spru941a).

    Do you have a simple application that is able to transmit EMAC packets in a way that matches your expectations?  We can use that as a starting point to isolate the problem.

     

    -Mike

  • yes I have included the dst and src addresses in header and I have tested the simple application to send ethernet packets :

    #include "emac.h"

    #define TX_BUF    1514//////
    #define RX_BUF    1536

    Uint8 packet_data[TX_BUF];
    void* ptr;//////
    Uint8 packet_buffer1[RX_BUF];
    Uint8 packet_buffer2[RX_BUF];
    Uint8 packet_buffer3[RX_BUF];
    Uint8 packet_buffer4[RX_BUF];
    Uint8 packet_buffer5[RX_BUF];
    Uint8 packet_buffer6[RX_BUF];
    Uint8 packet_buffer7[RX_BUF];
    Uint8 packet_buffer8[RX_BUF];
    Uint8 packet_buffer9[RX_BUF];
    Uint8 packet_buffer10[RX_BUF];

    /*
     *  We use pDescBase for a base address. Its easier this way
     *  because we can use indexing off the pointer.
     */
    EMAC_Desc* pDescBase = ( EMAC_Desc* )EMAC_RAM_BASE;

    /*
     *  The following are used to allow the ISR to communicate with
     *  the application.
     */
    extern volatile int RxCount;
    extern volatile int TxCount;
    extern volatile int ErrCount;
    extern volatile EMAC_Desc *pDescRx;
    extern volatile EMAC_Desc *pDescTx;
    extern Uint8* dest;
    Int16 verify_packet( EMAC_Desc* pDesc, Uint32 size, Uint32 flagCRC );

    /* ------------------------------------------------------------------------ *
     *                                                                          *
     *  emac_test                                                               *
     *      EMAC tests to send data to external loopback cable.                 *
     *                                                                          *
     * ------------------------------------------------------------------------ */
    Int16 emac_test( )
    {
        Int32 i;
        Int16 errors = 0;
        Uint32 status;

        Int32 emac_timeout = 0x100000;
        Int32 timeout;
        EMAC_Desc* pDesc;
     dest = (void*)dest;      //one frame data

        /* ---------------------------------------------------------------- *
         *                                                                  *
         *  Setup EMAC                                                      *
         *                                                                  *
         * ---------------------------------------------------------------- */
        emac_init( );
    * ---------------------------------------------------------------- *
         *         
                                                                  *
         *  Setup TX packets                                                *
         *      Send 2 copies of the same packet using different sizes      *
         *                                                                  *
         * ---------------------------------------------------------------- */
      packet_data[0]=0x00;//
      packet_data[1]=0x11;//
      packet_data[2]=0x2F;//
      packet_data[3]=0xF4;
      packet_data[4]=0x6F;
      packet_data[5]=0x28;
      packet_data[6]=0x00;
      packet_data[7]=0x0E;
      packet_data[8]=0x99;
      packet_data[9]=0x02;
      packet_data[10]=0x99;
      packet_data[11]=0x3C;
      packet_data[12]=0x08;
      packet_data[13]=0x09;
      packet_data[14]=0x00;
      packet_data[15]=0x00;
       // for ( i = 12 ; i < TX_BUF ; i++ )  ////////////////
       //     packet_data[i] = i;
      
     for (i=0 ; i<553; i++)/////
    { 

        ptr = & packet_data[16];
     memcpy(ptr, dest+1498 * i,1498);
        pDesc            = pDescBase + 10;
        pDesc->pNext     = 0;////////
        pDesc->pBuffer   = packet_data;
        pDesc->BufOffLen = 1514;
        pDesc->PktFlgLen = EMAC_DSC_FLAG_OWNER
                         | EMAC_DSC_FLAG_SOP
                         | EMAC_DSC_FLAG_EOP
                         | 1514;
     


          /*
         *  Start TX sending
         */
        pDescTx = pDescBase + 10;
        EMAC_TX0HDP = ( Uint32 )pDescTx;

        /* ---------------------------------------------------------------- *
         *                                                                  *
         *  Normally there would be a interrupt to service the EMAC RX/TX   *
         *  transmission.  Instead a short pause and manually call the ISR  *
         *  Interrupt Service Routine to check on the status.               *
         *                                                                  *
         *  You can later add in the ISR and the code to support.           *
         *                                                                  *
         * ---------------------------------------------------------------- */

        /* Busy period */
        _wait( 10000 );

        /* Manually check ISR, if using interrupts this will be done automatically */
        EMAC_isr( );
    }

  • Thanks Rutcha.  The example really helps me put your code snippet into context.

    Are you receiving the correct number of packets?

    Instead of the _wait() statement, can you try a while loop to poll for any of the following:
      a) while( pDesc->PktFlgLen | EMAC_DSC_FLAG_OWNER );
      b) while( EMAC_TX0CP != (Uint32) pDescTx );  /* EMAC_TX0CP should be zero before the packet is transmitted */
      c) tmpInt = EMAC_TXGOODFRAMES; while( EMAC_TXGOODFRAMES == tmpInt );

     

  • I've also just started working on communicating two evmdm6437 boards through ethernet, and for starters i need to know where can i find that emac.pjt project so needed for implementing this!

    Kindly help!