Do we have version of UBL that support SPI boot on DM365? The latest version from PSP does not seem to support it. Thanks.
http://processors.wiki.ti.com/index.php/DaVinci_PSP_03.01_GA_%28r37%29_Release_Notes
Prateek
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Do we have version of UBL that support SPI boot on DM365? The latest version from PSP does not seem to support it. Thanks.
http://processors.wiki.ti.com/index.php/DaVinci_PSP_03.01_GA_%28r37%29_Release_Notes
Prateek
Yes. We have SPI UBL on DM365.
Not sure why, but I don't see the code in the latest release:
http://arago-project.org/files/releases/davinci-psp_3.x.0.0-r37/sources/flash-utils-davinci.tar.gz
I can send the code if you need it.
Thanks,
Gaurav
Thanks Gaurav. It would be great if you can send SPI UBL to me directly.
Prateek
Hi Gaurav
We need to implement SPI UBL on DM365 as well - will it be possible for you to make the code and any supporting documentation available to us?
Also - will the UBL be able to load U-Boot from SPI as well?
Thanks
George
George,
Yes, UBL will download UBoot from SPI. I am working on to make an official release for the UBL.
Thanks,
Gaurav
Gaurav
Thanks for the prompt response!
When do you expect the release will be ready?
Can I assist in any way to expedite the release?
Regards
George
George,
I do not have an estimated date for the release yet. If you want a pre-release, please contact your local TI sales office. They will work out the details.
Thanks,
Gaurav
Hi,
I have the similar requirement for for a differnet processor (DM6467). I want to boot UBL, UBoot from SPI flash memory on DM6467 processor. Can you please suggest me what changes I need to do in UBL and UBoot source code?
Regards,
Krunal
Krunal,
For UBL and uBoot, you will have to write a driver that can read from the SPI. For flashing into SPI, write functionality is also required.
Thanks,
Gaurav
Hi,
Thanks for the reply. I have few more queries:
Regards,
Krunal
1. No its not supported in UBL for DM6467. Please post a message on the linux forum for UBoot/Linux implementation/questions.
2. You can download sample/test code from Spectrum Digital website (http://support.spectrumdigital.com/boards/evmdm6467/revf/) which can be modified to flash the code.
Thanks,
Gaurav
Hi Gaurav,
Any update on the release of DM365 boot from SPI flash support?
Todd
Hi, Gaurav. It would be great if you can send SPI UBL to me directly, my email is 394238147@qq.com , thank you very much.
Zibo,
SPI UBL for this device is not released officially. Please contact your local TI sales office if you want a copy.
Regards,
Gaurav