Part Number: 66AK2L06
I am designing a board and want to use both SPI2 and UART0. SPI2CLK is shared as a secondary function with UART0CTS. I don't need to use either UART0CTS or UART0RTS. I want to confirm that UART0RXD and UART0TXD can be used with the UART0CTS pin being used for SPI2CLK.
I have not been able to find any documentation on selecting the secondary pin functions and resolution of that selection (i.e. pin or device). I am sure that is available, could someone point me to it?
Thanks, Chip Weller